Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static InspectionMethodBuilder.PolarAngleModeTypes |
InspectionMethodBuilder.PolarAngleModeTypes.FULL
Full circumference
|
static InspectionMethodBuilder.PolarAngleModeTypes |
InspectionMethodBuilder.PolarAngleModeTypes.PARTIAL
Start point and end point
|
Modifier and Type | Method and Description |
---|---|
InspectionMethodBuilder.PolarAngleModeTypes |
InspectionPolarGridBuilder.angleMode()
Returns the angle mode
License requirements: None. |
InspectionMethodBuilder.PolarAngleModeTypes |
InspectionMethodBuilder.angleMode()
Returns the polar angle mode
License requirements: None. |
static InspectionMethodBuilder.PolarAngleModeTypes |
InspectionMethodBuilder.PolarAngleModeTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static InspectionMethodBuilder.PolarAngleModeTypes |
InspectionMethodBuilder.PolarAngleModeTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static InspectionMethodBuilder.PolarAngleModeTypes[] |
InspectionMethodBuilder.PolarAngleModeTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
InspectionPolarGridBuilder.setAngleMode(InspectionMethodBuilder.PolarAngleModeTypes angleMode)
License requirements: insp_programming ("INSPECTION PROGRAMMING") . |
void |
InspectionMethodBuilder.setAngleMode(InspectionMethodBuilder.PolarAngleModeTypes mode)
License requirements: insp_programming ("INSPECTION PROGRAMMING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.