public static class InspectionMethodBuilder.PolarAngleModeTypes extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_FULL
Full circumference
|
static int |
_PARTIAL
Start point and end point
|
static InspectionMethodBuilder.PolarAngleModeTypes |
FULL
Full circumference
|
static InspectionMethodBuilder.PolarAngleModeTypes |
PARTIAL
Start point and end point
|
Modifier and Type | Method and Description |
---|---|
static InspectionMethodBuilder.PolarAngleModeTypes |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static InspectionMethodBuilder.PolarAngleModeTypes |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static InspectionMethodBuilder.PolarAngleModeTypes[] |
values()
Returns an array that contains the values for this enum.
|
public static final InspectionMethodBuilder.PolarAngleModeTypes FULL
public static final InspectionMethodBuilder.PolarAngleModeTypes PARTIAL
public static final int _FULL
public static final int _PARTIAL
public static InspectionMethodBuilder.PolarAngleModeTypes valueOf(int value)
public static InspectionMethodBuilder.PolarAngleModeTypes valueOf(String name)
public static InspectionMethodBuilder.PolarAngleModeTypes[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.