Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static InspectionConstructedFeatureBuilder.DestPcsEnumType |
InspectionConstructedFeatureBuilder.DestPcsEnumType.ACTUAL_PCS
Use a user specified actual PCS as the destination
|
static InspectionConstructedFeatureBuilder.DestPcsEnumType |
InspectionConstructedFeatureBuilder.DestPcsEnumType.CURRENT_PCS
Use current PCS as the destination
|
static InspectionConstructedFeatureBuilder.DestPcsEnumType |
InspectionConstructedFeatureBuilder.DestPcsEnumType.NOMINAL_PCS
Use a user specified nominal PCS as the destination
|
Modifier and Type | Method and Description |
---|---|
InspectionConstructedFeatureBuilder.DestPcsEnumType |
InspectionConstructedFeatureBuilder.destinationPcsEnum()
Returns the destination part coordinate system type
License requirements: None. |
static InspectionConstructedFeatureBuilder.DestPcsEnumType |
InspectionConstructedFeatureBuilder.DestPcsEnumType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static InspectionConstructedFeatureBuilder.DestPcsEnumType |
InspectionConstructedFeatureBuilder.DestPcsEnumType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static InspectionConstructedFeatureBuilder.DestPcsEnumType[] |
InspectionConstructedFeatureBuilder.DestPcsEnumType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
InspectionConstructedFeatureBuilder.setDestinationPcsEnum(InspectionConstructedFeatureBuilder.DestPcsEnumType destinationPcsEnum)
License requirements: insp_programming ("INSPECTION PROGRAMMING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.