Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static InspectionConstructedFeatureBuilder.CurrentStateType |
InspectionConstructedFeatureBuilder.CurrentStateType.ACTUAL
Feature is an actual measured feature
|
static InspectionConstructedFeatureBuilder.CurrentStateType |
InspectionConstructedFeatureBuilder.CurrentStateType.NOMINAL
Feature is in its nominal (design) state
|
Modifier and Type | Method and Description |
---|---|
InspectionConstructedFeatureBuilder.CurrentStateType |
InspectionConstructedFeatureBuilder.currentStateEnum()
Returns the current feature state (nominal or actual)
License requirements: None. |
InspectionConstructedFeatureBuilder.CurrentStateType[] |
InspectionConstructedFeatureBuilder.getSubFeatureStates()
Get the current subfeature states.
|
static InspectionConstructedFeatureBuilder.CurrentStateType |
InspectionConstructedFeatureBuilder.CurrentStateType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static InspectionConstructedFeatureBuilder.CurrentStateType |
InspectionConstructedFeatureBuilder.CurrentStateType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static InspectionConstructedFeatureBuilder.CurrentStateType[] |
InspectionConstructedFeatureBuilder.CurrentStateType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
InspectionConstructedFeatureBuilder.setCurrentStateEnum(InspectionConstructedFeatureBuilder.CurrentStateType currentStateEnum)
License requirements: insp_programming ("INSPECTION PROGRAMMING") . |
void |
InspectionConstructedFeatureBuilder.setSubFeatureStates(InspectionConstructedFeatureBuilder.CurrentStateType[] subFeatureStates)
Set the current subfeature states.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.