Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static CylinderMillingBuilder.DiameterForHelixTypes |
CylinderMillingBuilder.DiameterForHelixTypes.DIAMETER
Helix Diameter
|
static CylinderMillingBuilder.DiameterForHelixTypes |
CylinderMillingBuilder.DiameterForHelixTypes.OFFSET_FROM_START_DIAMETER
Offset from Start Diameter
|
static CylinderMillingBuilder.DiameterForHelixTypes |
CylinderMillingBuilder.DiameterForHelixTypes.SPIRAL_THICKNESS
Spiral Thickness
|
Modifier and Type | Method and Description |
---|---|
CylinderMillingBuilder.DiameterForHelixTypes |
CylinderMillingBuilder.diameterForHelix()
Returns the Diameter for Helix
License requirements: None. |
static CylinderMillingBuilder.DiameterForHelixTypes |
CylinderMillingBuilder.DiameterForHelixTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CylinderMillingBuilder.DiameterForHelixTypes |
CylinderMillingBuilder.DiameterForHelixTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CylinderMillingBuilder.DiameterForHelixTypes[] |
CylinderMillingBuilder.DiameterForHelixTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
CylinderMillingBuilder.setDiameterForHelix(CylinderMillingBuilder.DiameterForHelixTypes newValue)
License requirements: cam_base ("CAM BASE") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.