public static class CylinderMillingBuilder.DiameterForHelixTypes extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_DIAMETER
Helix Diameter
|
static int |
_OFFSET_FROM_START_DIAMETER
Offset from Start Diameter
|
static int |
_SPIRAL_THICKNESS
Spiral Thickness
|
static CylinderMillingBuilder.DiameterForHelixTypes |
DIAMETER
Helix Diameter
|
static CylinderMillingBuilder.DiameterForHelixTypes |
OFFSET_FROM_START_DIAMETER
Offset from Start Diameter
|
static CylinderMillingBuilder.DiameterForHelixTypes |
SPIRAL_THICKNESS
Spiral Thickness
|
Modifier and Type | Method and Description |
---|---|
static CylinderMillingBuilder.DiameterForHelixTypes |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CylinderMillingBuilder.DiameterForHelixTypes |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CylinderMillingBuilder.DiameterForHelixTypes[] |
values()
Returns an array that contains the values for this enum.
|
public static final CylinderMillingBuilder.DiameterForHelixTypes DIAMETER
public static final CylinderMillingBuilder.DiameterForHelixTypes SPIRAL_THICKNESS
public static final CylinderMillingBuilder.DiameterForHelixTypes OFFSET_FROM_START_DIAMETER
public static final int _DIAMETER
public static final int _SPIRAL_THICKNESS
public static final int _OFFSET_FROM_START_DIAMETER
public static CylinderMillingBuilder.DiameterForHelixTypes valueOf(int value)
public static CylinderMillingBuilder.DiameterForHelixTypes valueOf(String name)
public static CylinderMillingBuilder.DiameterForHelixTypes[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.