Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static ChamferMillingBuilder.ChamferReferenceType |
ChamferMillingBuilder.ChamferReferenceType.MAX_DIAMETER
reference to max (C-Sink) diameter
|
static ChamferMillingBuilder.ChamferReferenceType |
ChamferMillingBuilder.ChamferReferenceType.MIN_DIAMETER
reference to min (Hole) diameter
|
Modifier and Type | Method and Description |
---|---|
ChamferMillingBuilder.ChamferReferenceType |
ChamferMillingBuilder.chamferReference()
Returns the chamfer reference
License requirements: None. |
static ChamferMillingBuilder.ChamferReferenceType |
ChamferMillingBuilder.ChamferReferenceType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ChamferMillingBuilder.ChamferReferenceType |
ChamferMillingBuilder.ChamferReferenceType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ChamferMillingBuilder.ChamferReferenceType[] |
ChamferMillingBuilder.ChamferReferenceType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ChamferMillingBuilder.setChamferReference(ChamferMillingBuilder.ChamferReferenceType chamferReference)
License requirements: cam_base ("CAM BASE") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.