public static class ChamferMillingBuilder.ChamferReferenceType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_MAX_DIAMETER
reference to max (C-Sink) diameter
|
static int |
_MIN_DIAMETER
reference to min (Hole) diameter
|
static ChamferMillingBuilder.ChamferReferenceType |
MAX_DIAMETER
reference to max (C-Sink) diameter
|
static ChamferMillingBuilder.ChamferReferenceType |
MIN_DIAMETER
reference to min (Hole) diameter
|
Modifier and Type | Method and Description |
---|---|
static ChamferMillingBuilder.ChamferReferenceType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ChamferMillingBuilder.ChamferReferenceType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ChamferMillingBuilder.ChamferReferenceType[] |
values()
Returns an array that contains the values for this enum.
|
public static final ChamferMillingBuilder.ChamferReferenceType MAX_DIAMETER
public static final ChamferMillingBuilder.ChamferReferenceType MIN_DIAMETER
public static final int _MAX_DIAMETER
public static final int _MIN_DIAMETER
public static ChamferMillingBuilder.ChamferReferenceType valueOf(int value)
public static ChamferMillingBuilder.ChamferReferenceType valueOf(String name)
public static ChamferMillingBuilder.ChamferReferenceType[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.