Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static BoundaryTurnBlank.Position |
BoundaryTurnBlank.Position.AT_HEADSTOCK |
static BoundaryTurnBlank.Position |
BoundaryTurnBlank.Position.AWAYFROM_HEADSTOCK |
Modifier and Type | Method and Description |
---|---|
BoundaryTurnBlank.Position |
BoundaryTurnBlank.mountingPosition()
Returns the mounting position
License requirements: None. |
static BoundaryTurnBlank.Position |
BoundaryTurnBlank.Position.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static BoundaryTurnBlank.Position |
BoundaryTurnBlank.Position.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static BoundaryTurnBlank.Position[] |
BoundaryTurnBlank.Position.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
BoundaryTurnBlank.setMountingPosition(BoundaryTurnBlank.Position mountPos)
License requirements: cam_base ("CAM BASE") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.