public static class BoundaryTurnBlank.Position extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_AT_HEADSTOCK |
static int |
_AWAYFROM_HEADSTOCK |
static BoundaryTurnBlank.Position |
AT_HEADSTOCK |
static BoundaryTurnBlank.Position |
AWAYFROM_HEADSTOCK |
Modifier and Type | Method and Description |
---|---|
static BoundaryTurnBlank.Position |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static BoundaryTurnBlank.Position |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static BoundaryTurnBlank.Position[] |
values()
Returns an array that contains the values for this enum.
|
public static final BoundaryTurnBlank.Position AT_HEADSTOCK
public static final BoundaryTurnBlank.Position AWAYFROM_HEADSTOCK
public static final int _AT_HEADSTOCK
public static final int _AWAYFROM_HEADSTOCK
public static BoundaryTurnBlank.Position valueOf(int value)
public static BoundaryTurnBlank.Position valueOf(String name)
public static BoundaryTurnBlank.Position[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.