Package | Description |
---|---|
nxopen.cae.responsesimulation |
Provides classes and interfaces for Response Simulation.
|
Modifier and Type | Field and Description |
---|---|
static VelocityImpactExcitationBuilder.ImpactMethodType |
VelocityImpactExcitationBuilder.ImpactMethodType.CONSTANT_VELOCITY
the users will only be able to specify the velocity for the impact
|
static VelocityImpactExcitationBuilder.ImpactMethodType |
VelocityImpactExcitationBuilder.ImpactMethodType.DROP_IMPACT
the users will be able to specify the drop height or the desired velocity at the impact
|
Modifier and Type | Method and Description |
---|---|
VelocityImpactExcitationBuilder.ImpactMethodType |
VelocityImpactExcitationBuilder.impactMethod()
Returns the impact method
License requirements: None. |
static VelocityImpactExcitationBuilder.ImpactMethodType |
VelocityImpactExcitationBuilder.ImpactMethodType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static VelocityImpactExcitationBuilder.ImpactMethodType |
VelocityImpactExcitationBuilder.ImpactMethodType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static VelocityImpactExcitationBuilder.ImpactMethodType[] |
VelocityImpactExcitationBuilder.ImpactMethodType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
VelocityImpactExcitationBuilder.setImpactMethod(VelocityImpactExcitationBuilder.ImpactMethodType impactMethod)
License requirements: nx_response_anlys ("NX Response Analysis") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.