public static class VelocityImpactExcitationBuilder.ImpactMethodType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_CONSTANT_VELOCITY
the users will only be able to specify the velocity for the impact
|
static int |
_DROP_IMPACT
the users will be able to specify the drop height or the desired velocity at the impact
|
static VelocityImpactExcitationBuilder.ImpactMethodType |
CONSTANT_VELOCITY
the users will only be able to specify the velocity for the impact
|
static VelocityImpactExcitationBuilder.ImpactMethodType |
DROP_IMPACT
the users will be able to specify the drop height or the desired velocity at the impact
|
Modifier and Type | Method and Description |
---|---|
static VelocityImpactExcitationBuilder.ImpactMethodType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static VelocityImpactExcitationBuilder.ImpactMethodType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static VelocityImpactExcitationBuilder.ImpactMethodType[] |
values()
Returns an array that contains the values for this enum.
|
public static final VelocityImpactExcitationBuilder.ImpactMethodType CONSTANT_VELOCITY
public static final VelocityImpactExcitationBuilder.ImpactMethodType DROP_IMPACT
public static final int _CONSTANT_VELOCITY
public static final int _DROP_IMPACT
public static VelocityImpactExcitationBuilder.ImpactMethodType valueOf(int value)
public static VelocityImpactExcitationBuilder.ImpactMethodType valueOf(String name)
public static VelocityImpactExcitationBuilder.ImpactMethodType[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.