Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
nxopen.cae.ftk |
Provides classes and interfaces to Function Toolkit.
|
Modifier and Type | Field and Description |
---|---|
static XyFunctionGeneralType |
XyFunctionGeneralType.CAMPBELL_DIAGRAM
Function is Campbell Diagram
|
static XyFunctionGeneralType |
XyFunctionGeneralType.CROSS_SPECTRUM
Function is Cross Spectrum
|
static XyFunctionGeneralType |
XyFunctionGeneralType.FAST_RMS_FITTED_PSD
Function is Fast RMS Fitted PSD
|
static XyFunctionGeneralType |
XyFunctionGeneralType.FREQUENCY_RESPONSE_FUNCTION
Function is Frequency Response Function
|
static XyFunctionGeneralType |
XyFunctionGeneralType.GENERAL
Function is General Function.
|
XyFunctionGeneralType |
FunctionBuilder.TypesData.generalType
Data type of function
|
static XyFunctionGeneralType |
XyFunctionGeneralType.LIFE
Function is Fatigue Life
|
static XyFunctionGeneralType |
XyFunctionGeneralType.MOTION_GENERAL
Function is Motion General Function
|
static XyFunctionGeneralType |
XyFunctionGeneralType.NUMBER
General Type Function Number
|
static XyFunctionGeneralType |
XyFunctionGeneralType.POWER_SPECTRAL_DENSITY
Function is Power Spectral Density
|
static XyFunctionGeneralType |
XyFunctionGeneralType.SHOCK_RESPONSE_SPECTRUM
Function is Shock Response Spectrum
|
static XyFunctionGeneralType |
XyFunctionGeneralType.SPECTRUM
Function is Spectrum
|
static XyFunctionGeneralType |
XyFunctionGeneralType.STIFFNESS_AND_DAMPING
Function is Stiffness and Damping
|
static XyFunctionGeneralType |
XyFunctionGeneralType.STRESS_STRAIN
Function is Stress/Strain Function
|
static XyFunctionGeneralType |
XyFunctionGeneralType.TEMPERATURE
Function is Temperature
|
static XyFunctionGeneralType |
XyFunctionGeneralType.TIME
Function is Time History
|
static XyFunctionGeneralType |
XyFunctionGeneralType.TIMING_CHART
Function is Timing Chart
|
static XyFunctionGeneralType |
XyFunctionGeneralType.TRANSMISSIBILITY
Function is Transmissibility
|
static XyFunctionGeneralType |
XyFunctionGeneralType.VEHICLE
Function is Vehicle
|
Modifier and Type | Method and Description |
---|---|
static XyFunctionGeneralType |
XyFunctionGeneralType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static XyFunctionGeneralType |
XyFunctionGeneralType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static XyFunctionGeneralType[] |
XyFunctionGeneralType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
String |
AfuManager.createRecord(XyFunctionMacroType macroType,
XyFunctionGeneralType dataType,
AfuData afuData)
Create a new AFU Data Record.
|
String |
AfuManager.editRecord(XyFunctionMacroType macroType,
XyFunctionGeneralType dataType,
int afuRecordIndex,
AfuData afuData)
Edit an existing AFU Data Record.
|
void |
FunctionBuilder.setTypes(Function.Type functionType,
XyFunctionMacroType macroType,
XyFunctionGeneralType generalType)
Sets types of a function
License requirements: None. |
Modifier and Type | Field and Description |
---|---|
XyFunctionGeneralType |
OptionSetting.RecordOptionData.functionType
Usage type of AFU Data Record used
|
Modifier and Type | Method and Description |
---|---|
void |
OptionSetting.setRecordOptionData(String recordName,
XyFunctionGeneralType functionType,
AfuData.AbscissaType abscissaType,
XyFunctionUnit xUnit,
AfuData.OrdinateType ordinateType,
XyFunctionUnit yUnit,
XyFunctionUnit yDenominatorUnit,
boolean sortValueType)
Set the record options data for an AFU Data Record
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.