public class XyFunctionMacroType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_GENERAL
Function could be used in any application
|
static int |
_LOAD
Function is only used to define a load
|
static int |
_MATERIAL
Function is only used to define a material
|
static int |
_MOTION
Function is only used in a motion application
|
static int |
_RESPONSE
Function is only used to define a response
|
static XyFunctionMacroType |
GENERAL
Function could be used in any application
|
static XyFunctionMacroType |
LOAD
Function is only used to define a load
|
static XyFunctionMacroType |
MATERIAL
Function is only used to define a material
|
static XyFunctionMacroType |
MOTION
Function is only used in a motion application
|
static XyFunctionMacroType |
RESPONSE
Function is only used to define a response
|
Modifier and Type | Method and Description |
---|---|
static XyFunctionMacroType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static XyFunctionMacroType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static XyFunctionMacroType[] |
values()
Returns an array that contains the values for this enum.
|
public static final XyFunctionMacroType GENERAL
public static final XyFunctionMacroType MOTION
public static final XyFunctionMacroType RESPONSE
public static final XyFunctionMacroType LOAD
public static final XyFunctionMacroType MATERIAL
public static final int _GENERAL
public static final int _MOTION
public static final int _RESPONSE
public static final int _LOAD
public static final int _MATERIAL
public static XyFunctionMacroType valueOf(int value)
public static XyFunctionMacroType valueOf(String name)
public static XyFunctionMacroType[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.