Modifier and Type | Interface and Description |
---|---|
static class |
OptionSetting.RecordOptionData
This class holds the data returned from
getRecordOptionData() |
Modifier and Type | Method and Description |
---|---|
boolean |
getHeaderFlag()
Get the adding header flag when export to CSV file
License requirements: None. |
OptionSetting.RecordOptionData |
getRecordOptionData()
Get the record options data for an AFU Data Record
License requirements: None. |
void |
setHeaderFlag(boolean addHeader)
Set the adding header flag when export to CSV file
License requirements: None. |
void |
setRecordOptionData(String recordName,
XyFunctionGeneralType functionType,
AfuData.AbscissaType abscissaType,
XyFunctionUnit xUnit,
AfuData.OrdinateType ordinateType,
XyFunctionUnit yUnit,
XyFunctionUnit yDenominatorUnit,
boolean sortValueType)
Set the record options data for an AFU Data Record
License requirements: None. |
OptionSetting.RecordOptionData getRecordOptionData() throws NXException, RemoteException
NXException
RemoteException
void setRecordOptionData(String recordName, XyFunctionGeneralType functionType, AfuData.AbscissaType abscissaType, XyFunctionUnit xUnit, AfuData.OrdinateType ordinateType, XyFunctionUnit yUnit, XyFunctionUnit yDenominatorUnit, boolean sortValueType) throws NXException, RemoteException
recordName
- The name of the AFU Data RecordfunctionType
- Usage type of AFU Data Record usedabscissaType
- Abscissa specific data typexUnit
- Unit Code of AFU dataordinateType
- Ordinate data typeyUnit
- Unit Code of AFU datayDenominatorUnit
- Unit Code of AFU datasortValueType
- If want to sort value in x directionNXException
RemoteException
boolean getHeaderFlag() throws NXException, RemoteException
NXException
RemoteException
void setHeaderFlag(boolean addHeader) throws NXException, RemoteException
addHeader
- If want to add header when export to CSV fileNXException
RemoteException
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.