Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static SimSolution.SetupCheckOption |
SimSolution.SetupCheckOption.CHECK_AND_STOP_AT_FIRST_ERROR
perform set up checks but stop at first error
|
static SimSolution.SetupCheckOption |
SimSolution.SetupCheckOption.COMPLETE_CHECK_AND_OUTPUT_ERRORS
perform all set up checks and report all errors
|
static SimSolution.SetupCheckOption |
SimSolution.SetupCheckOption.DO_NOT_CHECK
do perform any set up checks
|
Modifier and Type | Method and Description |
---|---|
static SimSolution.SetupCheckOption |
SimSolution.SetupCheckOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SimSolution.SetupCheckOption |
SimSolution.SetupCheckOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SimSolution.SetupCheckOption[] |
SimSolution.SetupCheckOption.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SimSolution.solve(SimSolution.SolveOption solveOption,
SimSolution.SetupCheckOption setupCheckOption)
Solves the solution
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
SimSolveManager.SolveAllMetaSolutionsData |
SimSolveManager.solveAllMetaSolutions(SimSolution.SolveOption solveOption,
SimSolution.SetupCheckOption setupCheckOption,
SimSolution.SolveMode runModeOption,
boolean skipSolutionWithResults)
Solve all meta solutions in the sim document.
|
SimSolveManager.SolveAllSolutionsData |
SimSolveManager.solveAllSolutions(SimSolution.SolveOption solveOption,
SimSolution.SetupCheckOption setupCheckOption,
SimSolution.SolveMode runModeOption,
boolean skipSolutionWithResults)
Solve all solutions in the sim document.
|
SimSolveManager.SolveChainOfSolutionsData |
SimSolveManager.solveChainOfSolutions(SimSolution[] pSolutions,
SimSolution.SolveOption solveOption,
SimSolution.SetupCheckOption setupCheckOption,
SimSolution.SolveMode runModeOption)
Solve the chain of solutions given in input.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.