Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static SetManager.DistributedPlanesBoundingSphereType |
SetManager.DistributedPlanesBoundingSphereType.FULL
places the distributed planes on a full sphere
|
static SetManager.DistributedPlanesBoundingSphereType |
SetManager.DistributedPlanesBoundingSphereType.HALF
places the distributed planes on half a sphere
|
SetManager.DistributedPlanesBoundingSphereType |
SetManager.TargetSetDistributedPlanesData.spacedefinition
Type of bounding sphere (half or full)
|
Modifier and Type | Method and Description |
---|---|
static SetManager.DistributedPlanesBoundingSphereType |
SetManager.DistributedPlanesBoundingSphereType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SetManager.DistributedPlanesBoundingSphereType |
SetManager.DistributedPlanesBoundingSphereType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SetManager.DistributedPlanesBoundingSphereType[] |
SetManager.DistributedPlanesBoundingSphereType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SetManager.setTargetSetDistributedPlanes(int setIndex,
SetManager.DistributedPlanesPosition centerMethod,
Point centerPoint,
SetManager.DistributedPlanesPosition radiusMethod,
Expression radiusFactor,
Expression radiusValue,
SetManager.DistributedPlanesBboxType bboxOption,
FEElement[] bboxElems,
SetManager.DistributedPlanesBoundingSphereType spaceDefinition,
SetManager.DistributedPlanesBoundingSphereDirection sphereDirection,
Direction sphereDirectionVector,
Point sphereDirectionPoint1,
Point sphereDirectionPoint2,
Point sphereDirectionPoint3,
boolean flipNormal,
int refinementLevel)
Sets the parameters for a distributed planes set.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.