public static class SetManager.DistributedPlanesBoundingSphereType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_FULL
places the distributed planes on a full sphere
|
static int |
_HALF
places the distributed planes on half a sphere
|
static SetManager.DistributedPlanesBoundingSphereType |
FULL
places the distributed planes on a full sphere
|
static SetManager.DistributedPlanesBoundingSphereType |
HALF
places the distributed planes on half a sphere
|
Modifier and Type | Method and Description |
---|---|
static SetManager.DistributedPlanesBoundingSphereType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SetManager.DistributedPlanesBoundingSphereType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SetManager.DistributedPlanesBoundingSphereType[] |
values()
Returns an array that contains the values for this enum.
|
public static final SetManager.DistributedPlanesBoundingSphereType HALF
public static final SetManager.DistributedPlanesBoundingSphereType FULL
public static final int _HALF
public static final int _FULL
public static SetManager.DistributedPlanesBoundingSphereType valueOf(int value)
public static SetManager.DistributedPlanesBoundingSphereType valueOf(String name)
public static SetManager.DistributedPlanesBoundingSphereType[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.