public static class SetManager.DistributedPlanesBboxType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_MODEL
the whole FE model is used to calculate the bounding box
|
static int |
_SELECTION
a selection of elements is used to define the bounding box
|
static SetManager.DistributedPlanesBboxType |
MODEL
the whole FE model is used to calculate the bounding box
|
static SetManager.DistributedPlanesBboxType |
SELECTION
a selection of elements is used to define the bounding box
|
Modifier and Type | Method and Description |
---|---|
static SetManager.DistributedPlanesBboxType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SetManager.DistributedPlanesBboxType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SetManager.DistributedPlanesBboxType[] |
values()
Returns an array that contains the values for this enum.
|
public static final SetManager.DistributedPlanesBboxType MODEL
public static final SetManager.DistributedPlanesBboxType SELECTION
public static final int _MODEL
public static final int _SELECTION
public static SetManager.DistributedPlanesBboxType valueOf(int value)
public static SetManager.DistributedPlanesBboxType valueOf(String name)
public static SetManager.DistributedPlanesBboxType[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.