Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
SetManager.DistributedPlanesBoundingSphereDirection |
SetManager.TargetSetDistributedPlanesData.spheredirection
Sphere direction definition method
|
static SetManager.DistributedPlanesBoundingSphereDirection |
SetManager.DistributedPlanesBoundingSphereDirection.THREE_POINTS_NORMAL
defines Z+ from 3 points that form a plane and a normal
|
static SetManager.DistributedPlanesBoundingSphereDirection |
SetManager.DistributedPlanesBoundingSphereDirection.VECTOR
defines Z+ with a vector
|
Modifier and Type | Method and Description |
---|---|
static SetManager.DistributedPlanesBoundingSphereDirection |
SetManager.DistributedPlanesBoundingSphereDirection.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SetManager.DistributedPlanesBoundingSphereDirection |
SetManager.DistributedPlanesBoundingSphereDirection.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SetManager.DistributedPlanesBoundingSphereDirection[] |
SetManager.DistributedPlanesBoundingSphereDirection.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SetManager.setTargetSetDistributedPlanes(int setIndex,
SetManager.DistributedPlanesPosition centerMethod,
Point centerPoint,
SetManager.DistributedPlanesPosition radiusMethod,
Expression radiusFactor,
Expression radiusValue,
SetManager.DistributedPlanesBboxType bboxOption,
FEElement[] bboxElems,
SetManager.DistributedPlanesBoundingSphereType spaceDefinition,
SetManager.DistributedPlanesBoundingSphereDirection sphereDirection,
Direction sphereDirectionVector,
Point sphereDirectionPoint1,
Point sphereDirectionPoint2,
Point sphereDirectionPoint3,
boolean flipNormal,
int refinementLevel)
Sets the parameters for a distributed planes set.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.