Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
SetManager.DistributedPlanesBboxType |
SetManager.TargetSetDistributedPlanesData.bboxoption
Bounding box definition option
|
static SetManager.DistributedPlanesBboxType |
SetManager.DistributedPlanesBboxType.MODEL
the whole FE model is used to calculate the bounding box
|
static SetManager.DistributedPlanesBboxType |
SetManager.DistributedPlanesBboxType.SELECTION
a selection of elements is used to define the bounding box
|
Modifier and Type | Method and Description |
---|---|
static SetManager.DistributedPlanesBboxType |
SetManager.DistributedPlanesBboxType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SetManager.DistributedPlanesBboxType |
SetManager.DistributedPlanesBboxType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SetManager.DistributedPlanesBboxType[] |
SetManager.DistributedPlanesBboxType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SetManager.setTargetSetDistributedPlanes(int setIndex,
SetManager.DistributedPlanesPosition centerMethod,
Point centerPoint,
SetManager.DistributedPlanesPosition radiusMethod,
Expression radiusFactor,
Expression radiusValue,
SetManager.DistributedPlanesBboxType bboxOption,
FEElement[] bboxElems,
SetManager.DistributedPlanesBoundingSphereType spaceDefinition,
SetManager.DistributedPlanesBoundingSphereDirection sphereDirection,
Direction sphereDirectionVector,
Point sphereDirectionPoint1,
Point sphereDirectionPoint2,
Point sphereDirectionPoint3,
boolean flipNormal,
int refinementLevel)
Sets the parameters for a distributed planes set.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.