Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static Post.Spectrum |
Post.Spectrum.GRAY_SCALE |
Post.Spectrum |
Post.Colorbar.spectrum |
static Post.Spectrum |
Post.Spectrum.STOP_LIGHT |
static Post.Spectrum |
Post.Spectrum.STRUCTURAL |
static Post.Spectrum |
Post.Spectrum.THERMAL |
Modifier and Type | Method and Description |
---|---|
static Post.Spectrum |
Post.Spectrum.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static Post.Spectrum |
Post.Spectrum.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static Post.Spectrum[] |
Post.Spectrum.values()
Returns an array that contains the values for this enum.
|
Constructor and Description |
---|
Colorbar(Post.Spectrum spectrumInitial,
boolean invertSpectrumInitial,
Post.Scale scaleInitial,
boolean automaticLevelInitial,
int numberOfLevelsInitial,
Post.Threshold thresholdInitial,
double thresholdMinimumInitial,
double thresholdMaximumInitial,
boolean showOverflowAboveInitial,
boolean showOverflowBelowInitial,
NXColor overflowAboveColorInitial,
NXColor overflowBelowColorInitial,
Post.Position positionInitial,
Post.LimitDisplay overflowInitial,
Post.LimitDisplay underflowInitial)
Constructor for the Colorbar object.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.