public static class Post.Position extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_LEFT |
static int |
_NONE |
static int |
_RIGHT |
static Post.Position |
LEFT |
static Post.Position |
NONE |
static Post.Position |
RIGHT |
Modifier and Type | Method and Description |
---|---|
static Post.Position |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static Post.Position |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static Post.Position[] |
values()
Returns an array that contains the values for this enum.
|
public static final Post.Position LEFT
public static final Post.Position RIGHT
public static final Post.Position NONE
public static final int _LEFT
public static final int _RIGHT
public static final int _NONE
public static Post.Position valueOf(int value)
public static Post.Position valueOf(String name)
public static Post.Position[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.