public static class Post.Scale extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_AUTOMATIC |
static int |
_LINEAR |
static int |
_LOGARITHMIC |
static Post.Scale |
AUTOMATIC |
static Post.Scale |
LINEAR |
static Post.Scale |
LOGARITHMIC |
Modifier and Type | Method and Description |
---|---|
static Post.Scale |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static Post.Scale |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static Post.Scale[] |
values()
Returns an array that contains the values for this enum.
|
public static final Post.Scale AUTOMATIC
public static final Post.Scale LINEAR
public static final Post.Scale LOGARITHMIC
public static final int _AUTOMATIC
public static final int _LINEAR
public static final int _LOGARITHMIC
public static Post.Scale valueOf(int value)
public static Post.Scale valueOf(String name)
public static Post.Scale[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.