public interface PostScenarioParameters extends TransientObject
PostScenarioParameters
used
to instanciate a PostScenarioBuilder
.
PostScenarioManager.newPostScenarioParameters()
Modifier and Type | Method and Description |
---|---|
IPostScenarioDataSource |
dataSource()
Deprecated.
Deprecated in NX12.0.0. Data Sources are now added through
PostScenarioManager.dataSources() . Alternatively, setPreferredDataSources(nxopen.cae.DataSource[]) can be used to configure the default configuration of a scenario. Setting this attribute has the same effect as SetPreferredDataSources(value).
|
PostScenarioDescriptor |
scenarioDescriptor()
Returns the scenario descriptor used by the post scenario.
|
void |
setDataSource(IPostScenarioDataSource dataSource)
Deprecated.
Deprecated in NX12.0.0. Data Sources are now added through
PostScenarioManager.dataSources() . Alternatively, setPreferredDataSources(nxopen.cae.DataSource[]) can be used to configure the default configuration of a scenario. Setting this attribute has the same effect as SetPreferredDataSources(value).
|
void |
setPreferredDataSources(DataSource[] dataSources)
Set preferred Data Sources to influence the default configuration of a scenario.
|
void |
setScenarioDescriptor(PostScenarioDescriptor scenarioDesc)
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
void |
setViewPortIndex(int viewPortIndex)
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
int |
viewPortIndex()
Returns the index of a view port on the main graphic window, on which the plot graph will be shown.
|
_value, dispose, printTestData, printTestData
PostScenarioDescriptor scenarioDescriptor() throws NXException, RemoteException
NXException
RemoteException
void setScenarioDescriptor(PostScenarioDescriptor scenarioDesc) throws NXException, RemoteException
scenarioDesc
- NXException
RemoteException
IPostScenarioDataSource dataSource() throws NXException, RemoteException
PostScenarioManager.dataSources()
. Alternatively, setPreferredDataSources(nxopen.cae.DataSource[])
can be used to configure the default configuration of a scenario. Setting this attribute has the same effect as SetPreferredDataSources(value).
NXException
RemoteException
void setDataSource(IPostScenarioDataSource dataSource) throws NXException, RemoteException
PostScenarioManager.dataSources()
. Alternatively, setPreferredDataSources(nxopen.cae.DataSource[])
can be used to configure the default configuration of a scenario. Setting this attribute has the same effect as SetPreferredDataSources(value).
dataSource
- NXException
RemoteException
int viewPortIndex() throws NXException, RemoteException
NXException
RemoteException
void setViewPortIndex(int viewPortIndex) throws NXException, RemoteException
viewPortIndex
- NXException
RemoteException
void setPreferredDataSources(DataSource[] dataSources) throws NXException, RemoteException
dataSources
- The data sources can be retrieved from PostScenarioManager.dataSources()
NXException
RemoteException
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.