Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Method and Description |
---|---|
PostScenarioParameters |
PostScenarioManager.newPostScenarioParameters()
Creates a transient object
PostScenarioParameters that
contains the settings required to create a post scenario. |
Modifier and Type | Method and Description |
---|---|
boolean |
PostScenarioManager.checkScenarioDataSourceCompatible(PostScenarioParameters scenarioParameters)
Deprecated.
Deprecated in NX12.0.0. This function is no longer useful because the new API only lists compatible data sources per slot.
|
boolean |
PostScenarioManager.checkValidDataSource(PostScenarioParameters scenarioParameters)
Checks if the data source set in
PostScenarioParameters is valid. |
PostScenarioBuilder |
PostScenarioManager.createPostScenarioBuilderFromParameters(PostScenarioParameters scenarioParameters)
Creates a transient object
PostScenarioBuilder that is
responsible for creating a post scenario object. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.