public interface PostScenarioSelectionParameters extends TaggedObject
PostScenarioInputDefinition
,
Data Source PostScenarioDataDefinition
, and PostScenarioVisualizationDefinition
. See PostScenarioBuilder
.
An instance can be created from a CAE.PostScenarioBuilder.
A valid user selection binds at least one value to each PostScenarioVariable
. The exact
constraints on the number of selected values varies which each scenario.
In order to bind values to variables, one must access each Variable from the
PostScenarioVariableCollection
, and bind values from those which are listed by the
Variable's PostScenarioVariable.getValues()
method.
PostScenarioConfigurationVariable
s are Scenario specific and enable or configure
scenario specific behaviour.
Modifier and Type | Method and Description |
---|---|
PostScenarioConfigurationVariableCollection |
configurationVariables()
Contains
PostScenarioConfigurationVariable s for this selection. |
void |
destroy()
Delete the
PostScenarioSelectionParameters . |
PostScenarioVariant |
newVariant()
Create a new
PostScenarioVariant that wraps a scalar value. |
void |
setIterationVariable(PostScenarioVariable variable)
Specifies which selection variable will be used for the next and previous quick-navigation commands.
|
PostScenarioVariableCollection |
variables()
Contains selection
PostScenarioVariable s that define this selection. |
printTestData, printTestData, tag, tagValue
PostScenarioVariableCollection variables() throws RemoteException
RemoteException
PostScenarioConfigurationVariableCollection configurationVariables() throws RemoteException
RemoteException
PostScenarioVariant newVariant() throws NXException, RemoteException
PostScenarioVariant
that wraps a scalar value. These objects need to be Dispose'd of once it is no longer needed.
NXException
RemoteException
void destroy() throws NXException, RemoteException
NXException
RemoteException
void setIterationVariable(PostScenarioVariable variable) throws NXException, RemoteException
variable
- NXException
RemoteException
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.