BushingBuilder Class¶
-
class
NXOpen.Motion.
BushingBuilder
¶ Bases:
NXOpen.Motion.MotionBuilder
Represents a Motion BushingBuilder
To create a new instance of this class, use
NXOpen.Motion.BushingCollection.CreateBushingBuilder()
Default values.
Property Value BushingActuatorCoefficients.CylindricalActuatorCoefficients.ConicalType Constant BushingActuatorCoefficients.CylindricalActuatorCoefficients.LongitudinalType Constant BushingActuatorCoefficients.CylindricalActuatorCoefficients.RadialType Constant BushingActuatorCoefficients.CylindricalActuatorCoefficients.TorsionalType Constant BushingActuatorCoefficients.GeneralTorsionalActuatorCoefficients.CoefficientsType Constant BushingActuatorCoefficients.GeneralTorsionalActuatorCoefficients.XCoefficientsType Constant BushingActuatorCoefficients.GeneralTorsionalActuatorCoefficients.YCoefficientsType Constant BushingActuatorCoefficients.GeneralTorsionalActuatorCoefficients.ZCoefficientsType Constant BushingDefine.AngleCalculation LargeAngle BushingDefine.ForceCalculation Abc BushingDefine.OrientationType Vector New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
BushingActuatorCoefficients | Returns the bushing actuator coefficients |
BushingCoefficients | Returns the bushing coefficients |
BushingDampingCoefficients | Returns the bushing damping coefficients |
BushingDefine | Returns the bushing define |
BushingStiffnessCoefficients | Returns the bushing stiffness coefficients |
BushingType | Returns or sets the type |
DisplayScale | Returns or sets the icon display scale |
GroupName | Returns or sets the group name |
GroupType | Returns or sets the group type |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
BushingBuilderBushingTypes Enumeration | Definitions of bushing type |
Property Detail¶
BushingActuatorCoefficients¶
-
BushingBuilder.
BushingActuatorCoefficients
¶ Returns the bushing actuator coefficients
-------------------------------------
Getter Method
Signature
BushingActuatorCoefficients
Returns: Return type: NXOpen.Motion.BushingActuatorCoefficients
New in version NX12.0.0.
License requirements: None.
BushingCoefficients¶
-
BushingBuilder.
BushingCoefficients
¶ Returns the bushing coefficients
-------------------------------------
Getter Method
Signature
BushingCoefficients
Returns: Return type: NXOpen.Motion.BushingCoefficients
New in version NX6.0.0.
Deprecated since version NX12.0.0: Obtain the coefficients using
Motion.BushingBuilder.BushingStiffnessCoefficients()
,Motion.BushingBuilder.BushingDampingCoefficients()
andMotion.BushingBuilder.BushingActuatorCoefficients()
to query or edit it.License requirements: None.
BushingDampingCoefficients¶
-
BushingBuilder.
BushingDampingCoefficients
¶ Returns the bushing damping coefficients
-------------------------------------
Getter Method
Signature
BushingDampingCoefficients
Returns: Return type: NXOpen.Motion.BushingDampingCoefficients
New in version NX12.0.0.
License requirements: None.
BushingDefine¶
-
BushingBuilder.
BushingDefine
¶ Returns the bushing define
-------------------------------------
Getter Method
Signature
BushingDefine
Returns: Return type: NXOpen.Motion.BushingDefine
New in version NX6.0.0.
License requirements: None.
BushingStiffnessCoefficients¶
-
BushingBuilder.
BushingStiffnessCoefficients
¶ Returns the bushing stiffness coefficients
-------------------------------------
Getter Method
Signature
BushingStiffnessCoefficients
Returns: Return type: NXOpen.Motion.BushingStiffnessCoefficients
New in version NX12.0.0.
License requirements: None.
BushingType¶
-
BushingBuilder.
BushingType
¶ Returns or sets the type
-------------------------------------
Getter Method
Signature
BushingType
Returns: Return type: NXOpen.Motion.BushingBuilderBushingTypes
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BushingType
Parameters: type ( NXOpen.Motion.BushingBuilderBushingTypes
) –New in version NX6.0.0.
License requirements: mechanisms (“MECHANISMS”)
Method Detail¶
Validate¶
-
BushingBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.