BushingActuatorCoefficients Class¶
-
class
NXOpen.Motion.
BushingActuatorCoefficients
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a Motion BushingActuatorCoefficients
New in version NX12.0.0.
Properties¶
Property | Description |
---|---|
CylindricalActuatorCoefficients | Returns the cylindrical actuator coefficients. |
GeneralTorsionalActuatorCoefficients | Returns the general torsional actuator coefficients. |
GeneralTranslationalActuatorCoefficients | Returns the general translational actuator coefficients. |
SphericalActuatorCoefficients | Returns the spherical actuator coefficients. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
CylindricalActuatorCoefficients¶
-
BushingActuatorCoefficients.
CylindricalActuatorCoefficients
¶ Returns the cylindrical actuator coefficients.
It is used in
Motion.BushingBuilderBushingTypes.Cylindrical
case-------------------------------------
Getter Method
Signature
CylindricalActuatorCoefficients
Returns: Return type: NXOpen.Motion.BushingCylindricalCoefficientsComponent
New in version NX12.0.0.
License requirements: None.
GeneralTorsionalActuatorCoefficients¶
-
BushingActuatorCoefficients.
GeneralTorsionalActuatorCoefficients
¶ Returns the general torsional actuator coefficients.
It is used in
Motion.BushingBuilderBushingTypes.General
case-------------------------------------
Getter Method
Signature
GeneralTorsionalActuatorCoefficients
Returns: Return type: NXOpen.Motion.BushingGeneralCoefficientsComponent
New in version NX12.0.0.
License requirements: None.
GeneralTranslationalActuatorCoefficients¶
-
BushingActuatorCoefficients.
GeneralTranslationalActuatorCoefficients
¶ Returns the general translational actuator coefficients.
It is used in
Motion.BushingBuilderBushingTypes.General
case-------------------------------------
Getter Method
Signature
GeneralTranslationalActuatorCoefficients
Returns: Return type: NXOpen.Motion.BushingGeneralCoefficientsComponent
New in version NX12.0.0.
License requirements: None.
SphericalActuatorCoefficients¶
-
BushingActuatorCoefficients.
SphericalActuatorCoefficients
¶ Returns the spherical actuator coefficients.
It is used in
Motion.BushingBuilderBushingTypes.Spherical
case-------------------------------------
Getter Method
Signature
SphericalActuatorCoefficients
Returns: Return type: NXOpen.Motion.BushingSphericalCoefficientsComponent
New in version NX12.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
BushingActuatorCoefficients.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.