BushingSphericalCoefficientsComponent Class¶
-
class
NXOpen.Motion.
BushingSphericalCoefficientsComponent
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a Motion BushingSphericalCoefficientsComponent
New in version NX12.0.0.
Properties¶
Property | Description |
---|---|
ConicalCurveProfile | Returns the conical curve profile. |
ConicalExpression | Returns the conical expression type |
ConicalFunction | Returns or sets the conical function type |
ConicalType | Returns or sets the conical coefficient type |
RadialCurveProfile | Returns the radial curve profile. |
RadialExpression | Returns the radial expression type |
RadialFunction | Returns or sets the radial function type |
RadialType | Returns or sets the radial type |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
ConicalCurveProfile¶
-
BushingSphericalCoefficientsComponent.
ConicalCurveProfile
¶ Returns the conical curve profile.
It is available only when
Motion.BushingSphericalCoefficientsComponent.ConicalType()
is set toMotionConnectorCoefficientTypes.Profile2d
orMotionConnectorCoefficientTypes.ExpressionAndProfile2d
-------------------------------------
Getter Method
Signature
ConicalCurveProfile
Returns: Return type: NXOpen.Motion.SelectFieldData
New in version NX12.0.0.
License requirements: mechanisms (“MECHANISMS”)
ConicalExpression¶
-
BushingSphericalCoefficientsComponent.
ConicalExpression
¶ Returns the conical expression type
-------------------------------------
Getter Method
Signature
ConicalExpression
Returns: Return type: NXOpen.Expression
New in version NX12.0.0.
License requirements: None.
ConicalFunction¶
-
BushingSphericalCoefficientsComponent.
ConicalFunction
¶ Returns or sets the conical function type
-------------------------------------
Getter Method
Signature
ConicalFunction
Returns: Return type: NXOpen.CAE.Function
New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ConicalFunction
Parameters: conicalFunction ( NXOpen.CAE.Function
) –New in version NX12.0.0.
License requirements: mechanisms (“MECHANISMS”)
ConicalType¶
-
BushingSphericalCoefficientsComponent.
ConicalType
¶ Returns or sets the conical coefficient type
-------------------------------------
Getter Method
Signature
ConicalType
Returns: Return type: NXOpen.Motion.ConnectorCoefficientTypes
New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ConicalType
Parameters: conicalType ( NXOpen.Motion.ConnectorCoefficientTypes
) –New in version NX12.0.0.
License requirements: mechanisms (“MECHANISMS”)
RadialCurveProfile¶
-
BushingSphericalCoefficientsComponent.
RadialCurveProfile
¶ Returns the radial curve profile.
It is available only when
Motion.BushingSphericalCoefficientsComponent.RadialType()
is set toMotionConnectorCoefficientTypes.Profile2d
orMotionConnectorCoefficientTypes.ExpressionAndProfile2d
-------------------------------------
Getter Method
Signature
RadialCurveProfile
Returns: Return type: NXOpen.Motion.SelectFieldData
New in version NX12.0.0.
License requirements: mechanisms (“MECHANISMS”)
RadialExpression¶
-
BushingSphericalCoefficientsComponent.
RadialExpression
¶ Returns the radial expression type
-------------------------------------
Getter Method
Signature
RadialExpression
Returns: Return type: NXOpen.Expression
New in version NX12.0.0.
License requirements: None.
RadialFunction¶
-
BushingSphericalCoefficientsComponent.
RadialFunction
¶ Returns or sets the radial function type
-------------------------------------
Getter Method
Signature
RadialFunction
Returns: Return type: NXOpen.CAE.Function
New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RadialFunction
Parameters: radialFunction ( NXOpen.CAE.Function
) –New in version NX12.0.0.
License requirements: mechanisms (“MECHANISMS”)
RadialType¶
-
BushingSphericalCoefficientsComponent.
RadialType
¶ Returns or sets the radial type
-------------------------------------
Getter Method
Signature
RadialType
Returns: Return type: NXOpen.Motion.ConnectorCoefficientTypes
New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RadialType
Parameters: radialType ( NXOpen.Motion.ConnectorCoefficientTypes
) –New in version NX12.0.0.
License requirements: mechanisms (“MECHANISMS”)
Method Detail¶
Validate¶
-
BushingSphericalCoefficientsComponent.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.