BushingDampingCoefficients Class¶
-
class
NXOpen.Motion.
BushingDampingCoefficients
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a Motion BushingDampingCoefficients
New in version NX12.0.0.
Properties¶
Property | Description |
---|---|
CylindricalDampingCoefficients | Returns the cylindrical damping coefficients. |
GeneralTorsionalDampingCoefficients | Returns the general torsional damping coefficients. |
GeneralTranslationalDampingCoefficients | Returns the general translational damping coefficients. |
SphericalDampingCoefficients | Returns the spherical damping coefficients. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
CylindricalDampingCoefficients¶
-
BushingDampingCoefficients.
CylindricalDampingCoefficients
¶ Returns the cylindrical damping coefficients.
It is used in
Motion.BushingBuilderBushingTypes.Cylindrical
case-------------------------------------
Getter Method
Signature
CylindricalDampingCoefficients
Returns: Return type: NXOpen.Motion.BushingCylindricalCoefficientsComponent
New in version NX12.0.0.
License requirements: None.
GeneralTorsionalDampingCoefficients¶
-
BushingDampingCoefficients.
GeneralTorsionalDampingCoefficients
¶ Returns the general torsional damping coefficients.
It is used in
Motion.BushingBuilderBushingTypes.General
case-------------------------------------
Getter Method
Signature
GeneralTorsionalDampingCoefficients
Returns: Return type: NXOpen.Motion.BushingGeneralCoefficientsComponent
New in version NX12.0.0.
License requirements: None.
GeneralTranslationalDampingCoefficients¶
-
BushingDampingCoefficients.
GeneralTranslationalDampingCoefficients
¶ Returns the general translational damping coefficients.
It is used in
Motion.BushingBuilderBushingTypes.General
case-------------------------------------
Getter Method
Signature
GeneralTranslationalDampingCoefficients
Returns: Return type: NXOpen.Motion.BushingGeneralCoefficientsComponent
New in version NX12.0.0.
License requirements: None.
SphericalDampingCoefficients¶
-
BushingDampingCoefficients.
SphericalDampingCoefficients
¶ Returns the spherical damping coefficients.
It is used in
Motion.BushingBuilderBushingTypes.Spherical
case-------------------------------------
Getter Method
Signature
SphericalDampingCoefficients
Returns: Return type: NXOpen.Motion.BushingSphericalCoefficientsComponent
New in version NX12.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
BushingDampingCoefficients.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.