BushingStiffnessCoefficients Class¶
-
class
NXOpen.Motion.
BushingStiffnessCoefficients
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a Motion BushingStiffnessCoefficients
New in version NX12.0.0.
Properties¶
Property | Description |
---|---|
CylindricalStiffnessCoefficients | Returns the cylindrical stiffness coefficients. |
GeneralTorsionalStiffnessCoefficients | Returns the general torsinal coefficients. |
GeneralTranslationalStiffnessCoefficients | Returns the general translational coefficients. |
SphericalStiffnessCoefficients | Returns the spherical coefficients. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
CylindricalStiffnessCoefficients¶
-
BushingStiffnessCoefficients.
CylindricalStiffnessCoefficients
¶ Returns the cylindrical stiffness coefficients.
It is used in
Motion.BushingBuilderBushingTypes.Cylindrical
case-------------------------------------
Getter Method
Signature
CylindricalStiffnessCoefficients
Returns: Return type: NXOpen.Motion.BushingCylindricalCoefficientsComponent
New in version NX12.0.0.
License requirements: None.
GeneralTorsionalStiffnessCoefficients¶
-
BushingStiffnessCoefficients.
GeneralTorsionalStiffnessCoefficients
¶ Returns the general torsinal coefficients.
It is used in
Motion.BushingBuilderBushingTypes.General
case-------------------------------------
Getter Method
Signature
GeneralTorsionalStiffnessCoefficients
Returns: Return type: NXOpen.Motion.BushingGeneralCoefficientsComponent
New in version NX12.0.0.
License requirements: None.
GeneralTranslationalStiffnessCoefficients¶
-
BushingStiffnessCoefficients.
GeneralTranslationalStiffnessCoefficients
¶ Returns the general translational coefficients.
It is used in
Motion.BushingBuilderBushingTypes.General
case-------------------------------------
Getter Method
Signature
GeneralTranslationalStiffnessCoefficients
Returns: Return type: NXOpen.Motion.BushingGeneralCoefficientsComponent
New in version NX12.0.0.
License requirements: None.
SphericalStiffnessCoefficients¶
-
BushingStiffnessCoefficients.
SphericalStiffnessCoefficients
¶ Returns the spherical coefficients.
It is used in
Motion.BushingBuilderBushingTypes.Spherical
case-------------------------------------
Getter Method
Signature
SphericalStiffnessCoefficients
Returns: Return type: NXOpen.Motion.BushingSphericalCoefficientsComponent
New in version NX12.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
BushingStiffnessCoefficients.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.