BushingCoefficients Class¶
-
class
NXOpen.Motion.
BushingCoefficients
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a Motion BushingCoefficients
New in version NX6.0.0.
Deprecated since version NX12.0.0: Use
Motion.BushingStiffnessCoefficients
,Motion.BushingDampingCoefficients
andMotion.BushingActuatorCoefficients
instead.
Properties¶
Property | Description |
---|---|
CylindricalCoefficients | Returns the cylindrical coefficients. |
SphericalCoefficients | Returns the spherical coefficients. |
Tag | Returns the Tag for this object. |
TorsionalCoefficients | Returns the torsional coefficients. |
TranslationalCoefficients | Returns the translational coefficients. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
CylindricalCoefficients¶
-
BushingCoefficients.
CylindricalCoefficients
¶ Returns the cylindrical coefficients.
It is used in
Motion.BushingBuilderBushingTypes.Cylindrical
case-------------------------------------
Getter Method
Signature
CylindricalCoefficients
Returns: Return type: NXOpen.Motion.BushingCylindricalCoefficients
New in version NX6.0.0.
License requirements: None.
SphericalCoefficients¶
-
BushingCoefficients.
SphericalCoefficients
¶ Returns the spherical coefficients.
It is used in
Motion.BushingBuilderBushingTypes.Spherical
case-------------------------------------
Getter Method
Signature
SphericalCoefficients
Returns: Return type: NXOpen.Motion.BushingSphericalCoefficients
New in version NX12.0.0.
License requirements: None.
TorsionalCoefficients¶
-
BushingCoefficients.
TorsionalCoefficients
¶ Returns the torsional coefficients.
It is used in
Motion.BushingBuilderBushingTypes.General
case-------------------------------------
Getter Method
Signature
TorsionalCoefficients
Returns: Return type: NXOpen.Motion.BushingGeneralCoefficients
New in version NX6.0.0.
License requirements: None.
TranslationalCoefficients¶
-
BushingCoefficients.
TranslationalCoefficients
¶ Returns the translational coefficients.
It is used in
Motion.BushingBuilderBushingTypes.General
case-------------------------------------
Getter Method
Signature
TranslationalCoefficients
Returns: Return type: NXOpen.Motion.BushingGeneralCoefficients
New in version NX6.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
BushingCoefficients.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.