AssignCornerBuilder Class¶
-
class
NXOpen.MechanicalRouting.
AssignCornerBuilder
¶ Bases:
NXOpen.Builder
Builder class for Assign Corner which creates corner
To create a new instance of this class, use
NXOpen.MechanicalRouting.BuilderFactory.CreateAssignCornerBuilder()
Default values.
Property Value BendCornerSettings.Method (deprecated) Radius BendCornerSettings.Radius.Value (deprecated) 0 (millimeters part), 0 (inches part) BendCornerSettings.RatioToDiameter.Value (deprecated) 0 (millimeters part), 0 (inches part) CornerSettings.CornerType None New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
BendCornerSettings | Returns the bend corner block |
ControlPointSelection | Returns the routing control points collector |
CornerSettings | Returns the corner block |
Tag | Returns the Tag for this object. |
Type | Returns or sets the assign corner type |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetCreatedComponents | Components created during Assign Corner operation. |
GetLogicalObjects | Returns the PDM.LogicalObject that represent the content that will be created by this builder. |
GetObject | Returns the object currently being edited by this builder. |
PreCommit | Performs the operations needed prior to a commit. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
AssignCornerBuilderCornerType Enumeration | Defines the corner types. |
Property Detail¶
BendCornerSettings¶
-
AssignCornerBuilder.
BendCornerSettings
¶ Returns the bend corner block
-------------------------------------
Getter Method
Signature
BendCornerSettings
Returns: Return type: NXOpen.MechanicalRouting.BendCornerTypeBuilder
New in version NX11.0.0.
Deprecated since version NX11.0.1: Use
NXOpen.MechanicalRouting.AssignCornerBuilder.CornerSettings()
instead.License requirements: routing_base (“Routing Basic”)
ControlPointSelection¶
-
AssignCornerBuilder.
ControlPointSelection
¶ Returns the routing control points collector
-------------------------------------
Getter Method
Signature
ControlPointSelection
Returns: Return type: NXOpen.Routing.RouteObjectCollector
New in version NX11.0.0.
License requirements: routing_base (“Routing Basic”)
CornerSettings¶
-
AssignCornerBuilder.
CornerSettings
¶ Returns the corner block
-------------------------------------
Getter Method
Signature
CornerSettings
Returns: Return type: NXOpen.MechanicalRouting.CornerBuilder
New in version NX11.0.1.
License requirements: routing_base (“Routing Basic”)
Type¶
-
AssignCornerBuilder.
Type
¶ Returns or sets the assign corner type
-------------------------------------
Getter Method
Signature
Type
Returns: Return type: NXOpen.MechanicalRouting.AssignCornerBuilderCornerType
New in version NX11.0.0.
Deprecated since version NX11.0.1: Use
NXOpen.MechanicalRouting.CornerBuilder.CornerType()
instead.License requirements: routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
Type
Parameters: type ( NXOpen.MechanicalRouting.AssignCornerBuilderCornerType
) –New in version NX11.0.0.
Deprecated since version NX11.0.1: Use
NXOpen.MechanicalRouting.CornerBuilder.CornerType()
instead.License requirements: routing_base (“Routing Basic”)
Method Detail¶
GetCreatedComponents¶
-
AssignCornerBuilder.
GetCreatedComponents
¶ Components created during Assign Corner operation.
Signature
GetCreatedComponents()
Returns: Components created during Assign Corner operation. Return type: list of NXOpen.Assemblies.Component
New in version NX11.0.1.
License requirements: routing_base (“Routing Basic”)
GetLogicalObjects¶
-
AssignCornerBuilder.
GetLogicalObjects
¶ Returns the
PDM.LogicalObject
that represent the content that will be created by this builder.logical objects will be created only for miter corner case.
Signature
GetLogicalObjects()
Returns: Return type: list of NXOpen.PDM.LogicalObject
New in version NX11.0.1.
License requirements: routing_base (“Routing Basic”)
PreCommit¶
-
AssignCornerBuilder.
PreCommit
¶ Performs the operations needed prior to a commit.
This method has to be called before invoking commit.
Signature
PreCommit()
New in version NX11.0.1.
License requirements: routing_base (“Routing Basic”)
Validate¶
-
AssignCornerBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.