AssignCornerBuilderCornerType Enumeration¶
NXOpen.MechanicalRouting.AssignCornerBuilder.CornerType is an alias for NXOpen.MechanicalRouting.AssignCornerBuilderCornerType
-
class
NXOpen.MechanicalRouting.
AssignCornerBuilderCornerType
¶ Bases:
object
Defines the corner types. None, Miter and Bend.
Deprecated since version NX11.0.1: Use
NXOpen.MechanicalRouting.CornerBuilderType
instead.Enum Members
Enum Member Enum Member Description NotSet Bend Miter -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-