CornerBuilderType Enumeration¶
NXOpen.MechanicalRouting.CornerBuilder.Type is an alias for NXOpen.MechanicalRouting.CornerBuilderType
-
class
NXOpen.MechanicalRouting.
CornerBuilderType
¶ Bases:
object
Corner Types available.
Enum Members
Enum Member Enum Member Description NotSet None, no corner created Bend allows corner creation with the specified bend type Miter allows miter corner creation -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-