CornerBuilder Class¶
-
class
NXOpen.MechanicalRouting.
CornerBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Builder class for Corner Block
New in version NX11.0.1.
Properties¶
Property | Description |
---|---|
BendCornerSettings | Returns the bend corner block |
CornerType | Returns or sets the corner types |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
CornerBuilderType Enumeration | Corner Types available. |
Property Detail¶
BendCornerSettings¶
-
CornerBuilder.
BendCornerSettings
¶ Returns the bend corner block
-------------------------------------
Getter Method
Signature
BendCornerSettings
Returns: Return type: NXOpen.MechanicalRouting.BendCornerTypeBuilder
New in version NX11.0.1.
License requirements: routing_base (“Routing Basic”)
CornerType¶
-
CornerBuilder.
CornerType
¶ Returns or sets the corner types
-------------------------------------
Getter Method
Signature
CornerType
Returns: Return type: NXOpen.MechanicalRouting.CornerBuilderType
New in version NX11.0.1.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
CornerType
Parameters: cornerType ( NXOpen.MechanicalRouting.CornerBuilderType
) –New in version NX11.0.1.
License requirements: routing_base (“Routing Basic”)
Method Detail¶
Validate¶
-
CornerBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.