BendCornerTypeBuilder Class¶
-
class
NXOpen.MechanicalRouting.
BendCornerTypeBuilder
¶ Bases:
NXOpen.MechanicalRouting.BaseCornerTypeBuilder
Contains setting for corner creation.
Type of bend to be created and the method to create the corner.
New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
BendTable | Returns or sets the name of bend radius table |
Method | Returns or sets the bend corner methods |
Radius | Returns the bend corner radius |
RatioToDiameter | Returns the bend corner ratio to diameter |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
ImportBendRadiusTable | Imports bend radius table |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
BendCornerTypeBuilderBendMethod Enumeration | Methods available for bend creation. |
Property Detail¶
BendTable¶
-
BendCornerTypeBuilder.
BendTable
¶ Returns or sets the name of bend radius table
-------------------------------------
Getter Method
Signature
BendTable
Returns: Return type: str New in version NX11.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
BendTable
Parameters: bendTableName (str) – New in version NX11.0.0.
License requirements: routing_base (“Routing Basic”)
Method¶
-
BendCornerTypeBuilder.
Method
¶ Returns or sets the bend corner methods
-------------------------------------
Getter Method
Signature
Method
Returns: Return type: NXOpen.MechanicalRouting.BendCornerTypeBuilderBendMethod
New in version NX11.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
Method
Parameters: routeCornerBendMethods ( NXOpen.MechanicalRouting.BendCornerTypeBuilderBendMethod
) –New in version NX11.0.0.
License requirements: routing_base (“Routing Basic”)
Radius¶
-
BendCornerTypeBuilder.
Radius
¶ Returns the bend corner radius
-------------------------------------
Getter Method
Signature
Radius
Returns: Return type: NXOpen.Expression
New in version NX11.0.0.
License requirements: routing_base (“Routing Basic”)
RatioToDiameter¶
-
BendCornerTypeBuilder.
RatioToDiameter
¶ Returns the bend corner ratio to diameter
-------------------------------------
Getter Method
Signature
RatioToDiameter
Returns: Return type: NXOpen.Expression
New in version NX11.0.0.
License requirements: routing_base (“Routing Basic”)
Method Detail¶
ImportBendRadiusTable¶
-
BendCornerTypeBuilder.
ImportBendRadiusTable
¶ Imports bend radius table
Signature
ImportBendRadiusTable(bendTableFilename)
Parameters: bendTableFilename (str) – New in version NX11.0.0.
License requirements: routing_base (“Routing Basic”)
Validate¶
-
BendCornerTypeBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.