BendCornerTypeBuilderBendMethod Enumeration¶
NXOpen.MechanicalRouting.BendCornerTypeBuilder.BendMethod is an alias for NXOpen.MechanicalRouting.BendCornerTypeBuilderBendMethod
-
class
NXOpen.MechanicalRouting.
BendCornerTypeBuilderBendMethod
¶ Bases:
object
Methods available for bend creation.
Enum Members
Enum Member Enum Member Description Radius Radius method allows corner creation with the specified radius value RatioToDiameter Ratio to diameter method BendRadiusTable Bend table method creates bend from specified bend table InnerRadius Inner Radius method allows corner creation with the specified inner radius value -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-