RouteObjectCollector Class¶
-
class
NXOpen.Routing.
RouteObjectCollector
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a
NXOpen.Routing.RouteObjectCollector
class to create objects for getting routing objects.New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
RoutingObjects | Returns the selected routing object list |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
RoutingObjects¶
-
RouteObjectCollector.
RoutingObjects
¶ Returns the selected routing object list
-------------------------------------
Getter Method
Signature
RoutingObjects
Returns: Return type: NXOpen.SelectNXObjectList
New in version NX6.0.0.
License requirements: routing_base (“Routing Basic”)
Method Detail¶
Validate¶
-
RouteObjectCollector.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.