WheelFixingBuilder Class¶
-
class
NXOpen.Features.VehicleDesign.
WheelFixingBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Features.VehicleDesign.WheelFixing
builder used to create or edit a vehicle design wheel fixing.To create a new instance of this class, use
NXOpen.Features.VehicleDesignCollection.CreateWheelFixingBuilder()
Default values.
Property Value HeightZ.Value 0 LengthX.Value 0 LevelZ.Value 0 ObjectPosition WheelExtents Position Front Radius.Value 0 RequirementsControl StandardDriven Shape Block WheelSize StaticRadius WidthY.Value 0 New in version NX8.5.0.
Properties¶
Property | Description |
---|---|
HeightZ | Returns the expression that contains the value which indicates the height Z of the wheel fixing when the shape is block. |
LengthX | Returns the expression that contains the value which indicates the Length X of the wheel fixing when the shape is block. |
LevelZ | Returns the expression that contains the value which indicates the level Z of the wheel fixing when the shape is circle segment. |
Loading | Returns or sets the loading used in the wheel fixing. |
ObjectPosition | Returns or sets the wheel fixing object position. |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
Position | Returns or sets the wheel fixing position. |
Radius | Returns the expression that contains the value which indicates the radius of the wheel fixing when the shape is circle segment. |
RequirementsControl | Returns or sets the requirements control for standard driven or user defined. |
Shape | Returns or sets the wheel fixing shape. |
Standard | Returns or sets the standard used to define the wheel fixing. |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
WheelSize | Returns or sets the wheel size of the wheel fixing. |
WidthY | Returns the expression that contains the value which indicates the Width Y of the wheel fixing when the shape is block. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
WheelFixingBuilderObjectPositionType Enumeration | Represents the object position used to indicate if the wheel fixing is positioned at the theoretically widest dimension of the wheel (diameter) or exactly at the wheel geometry of the base data. |
WheelFixingBuilderPositionType Enumeration | Represents the wheel fixing positions. |
WheelFixingBuilderRequirementsControlType Enumeration | Represents the requirements control types to define the wheel fixing. |
WheelFixingBuilderShapeType Enumeration | Represents the shape used to indicate if the wheel fixing is a block or a circle segment. |
WheelFixingBuilderWheelSizeType Enumeration | Represents the wheel size used to indicate if the wheel fixing is based on static radius or the diameter of the wheels. |
Property Detail¶
HeightZ¶
-
WheelFixingBuilder.
HeightZ
¶ Returns the expression that contains the value which indicates the height Z of the wheel fixing when the shape is block.
-------------------------------------
Getter Method
Signature
HeightZ
Returns: Return type: NXOpen.Expression
New in version NX8.5.0.
License requirements: None.
LengthX¶
-
WheelFixingBuilder.
LengthX
¶ Returns the expression that contains the value which indicates the Length X of the wheel fixing when the shape is block.
-------------------------------------
Getter Method
Signature
LengthX
Returns: Return type: NXOpen.Expression
New in version NX8.5.0.
License requirements: None.
LevelZ¶
-
WheelFixingBuilder.
LevelZ
¶ Returns the expression that contains the value which indicates the level Z of the wheel fixing when the shape is circle segment.
-------------------------------------
Getter Method
Signature
LevelZ
Returns: Return type: NXOpen.Expression
New in version NX8.5.0.
License requirements: None.
Loading¶
-
WheelFixingBuilder.
Loading
¶ Returns or sets the loading used in the wheel fixing.
-------------------------------------
Getter Method
Signature
Loading
Returns: Return type: str New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Loading
Parameters: loading (str) – New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
ObjectPosition¶
-
WheelFixingBuilder.
ObjectPosition
¶ Returns or sets the wheel fixing object position.
-------------------------------------
Getter Method
Signature
ObjectPosition
Returns: Return type: NXOpen.Features.VehicleDesign.WheelFixingBuilderObjectPositionType
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ObjectPosition
Parameters: objectPosition ( NXOpen.Features.VehicleDesign.WheelFixingBuilderObjectPositionType
) –New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
Position¶
-
WheelFixingBuilder.
Position
¶ Returns or sets the wheel fixing position.
-------------------------------------
Getter Method
Signature
Position
Returns: Return type: NXOpen.Features.VehicleDesign.WheelFixingBuilderPositionType
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Position
Parameters: position ( NXOpen.Features.VehicleDesign.WheelFixingBuilderPositionType
) –New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
Radius¶
-
WheelFixingBuilder.
Radius
¶ Returns the expression that contains the value which indicates the radius of the wheel fixing when the shape is circle segment.
-------------------------------------
Getter Method
Signature
Radius
Returns: Return type: NXOpen.Expression
New in version NX8.5.0.
License requirements: None.
RequirementsControl¶
-
WheelFixingBuilder.
RequirementsControl
¶ Returns or sets the requirements control for standard driven or user defined.
-------------------------------------
Getter Method
Signature
RequirementsControl
Returns: Return type: NXOpen.Features.VehicleDesign.WheelFixingBuilderRequirementsControlType
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RequirementsControl
Parameters: requirementsControl ( NXOpen.Features.VehicleDesign.WheelFixingBuilderRequirementsControlType
) –New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
Shape¶
-
WheelFixingBuilder.
Shape
¶ Returns or sets the wheel fixing shape.
-------------------------------------
Getter Method
Signature
Shape
Returns: Return type: NXOpen.Features.VehicleDesign.WheelFixingBuilderShapeType
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Shape
Parameters: shape ( NXOpen.Features.VehicleDesign.WheelFixingBuilderShapeType
) –New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
Standard¶
-
WheelFixingBuilder.
Standard
¶ Returns or sets the standard used to define the wheel fixing.
Only used when the requirements control type is
NXOpen.Features.VehicleDesign.WheelFixingBuilderRequirementsControlType.StandardDriven
.-------------------------------------
Getter Method
Signature
Standard
Returns: Return type: str New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Standard
Parameters: standard (str) – New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
WheelSize¶
-
WheelFixingBuilder.
WheelSize
¶ Returns or sets the wheel size of the wheel fixing.
-------------------------------------
Getter Method
Signature
WheelSize
Returns: Return type: NXOpen.Features.VehicleDesign.WheelFixingBuilderWheelSizeType
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
WheelSize
Parameters: wheelSize ( NXOpen.Features.VehicleDesign.WheelFixingBuilderWheelSizeType
) –New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
WidthY¶
-
WheelFixingBuilder.
WidthY
¶ Returns the expression that contains the value which indicates the Width Y of the wheel fixing when the shape is block.
-------------------------------------
Getter Method
Signature
WidthY
Returns: Return type: NXOpen.Expression
New in version NX8.5.0.
License requirements: None.
Method Detail¶
Validate¶
-
WheelFixingBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.