WheelFixingBuilderShapeType Enumeration

NXOpen.Features.VehicleDesign.WheelFixingBuilder.ShapeType is an alias for NXOpen.Features.VehicleDesign.WheelFixingBuilderShapeType

class NXOpen.Features.VehicleDesign.WheelFixingBuilderShapeType

Bases: object

Represents the shape used to indicate if the wheel fixing is a block or a circle segment.

Enum Members

Enum Member Enum Member Description
Block
CircleSegment
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.