WheelFixingBuilderWheelSizeType Enumeration

NXOpen.Features.VehicleDesign.WheelFixingBuilder.WheelSizeType is an alias for NXOpen.Features.VehicleDesign.WheelFixingBuilderWheelSizeType

class NXOpen.Features.VehicleDesign.WheelFixingBuilderWheelSizeType

Bases: object

Represents the wheel size used to indicate if the wheel fixing is based on static radius or the diameter of the wheels.

Enum Members

Enum Member Enum Member Description
StaticRadius
Diameter
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.