WheelFixingBuilderObjectPositionType Enumeration¶
NXOpen.Features.VehicleDesign.WheelFixingBuilder.ObjectPositionType is an alias for NXOpen.Features.VehicleDesign.WheelFixingBuilderObjectPositionType
-
class
NXOpen.Features.VehicleDesign.
WheelFixingBuilderObjectPositionType
¶ Bases:
object
Represents the object position used to indicate if the wheel fixing is positioned at the theoretically widest dimension of the wheel (diameter) or exactly at the wheel geometry of the base data.
Enum Members
Enum Member Enum Member Description WheelExtents WheelContact -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-