WheelCoveringBuilder Class¶
-
class
NXOpen.Features.VehicleDesign.
WheelCoveringBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Features.VehicleDesign.WheelCovering
feature builder for wheel covering surface section checking.To create a new instance of this class, use
NXOpen.Features.VehicleDesignCollection.CreateWheelCoveringBuilder()
New in version NX8.5.0.
Properties¶
Property | Description |
---|---|
DisplayIntersectionCurves | Returns or sets the display of the intersection curves. |
FrontBottomOffset | Returns the bottom offset of the front surface section when the front surface section type is NXOpen.Features.VehicleDesign.WheelCoveringBuilderSurfaceSectionType.Adr42 . |
FrontClearance | Returns the clearance of the front surface section. |
FrontFrontAngle | Returns the front angle of the front surface section. |
FrontFrontOffset | Returns the front offset of the front surface section when the front surface section type is NXOpen.Features.VehicleDesign.WheelCoveringBuilderSurfaceSectionType.Adr42 . |
FrontHeight | Returns the height of the front surface section when front the surface section type is NXOpen.Features.VehicleDesign.WheelCoveringBuilderSurfaceSectionType.Adr42 . |
FrontHubcapSelection | Returns the front hub cap selection. |
FrontObjectSelection | Returns the front object selection. |
FrontRadius | Returns the radius of the front surface section when the front surface section type is NXOpen.Features.VehicleDesign.WheelCoveringBuilderSurfaceSectionType.CircleSection . |
FrontRearAngle | Returns the rear angle of the front surface section. |
FrontRearOffset | Returns the rear offset of the front surface section when the front surface section type is NXOpen.Features.VehicleDesign.WheelCoveringBuilderSurfaceSectionType.Adr42 . |
FrontSurfacePlane | Returns or sets the surface plane type of the front surface section. |
FrontSurfaceSection | Returns or sets the surface section type of the front surface section. |
Loading | Returns or sets the loading used in the wheel covering. |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
Position | Returns or sets the wheel covering position. |
RearBottomOffset | Returns the bottom offset of the rear surface section when the rear surface section type is NXOpen.Features.VehicleDesign.WheelCoveringBuilderSurfaceSectionType.Adr42 . |
RearClearance | Returns the clearance of the rear surface section. |
RearDisToWheelCenter | Returns the distance to the wheel center when rear surface section type is NXOpen.Features.VehicleDesign.WheelCoveringBuilderSurfaceSectionType.CircleSection . |
RearFrontAngle | Returns the front angle of the rear surface section. |
RearFrontOffset | Returns the front offset of the rear surface section when the rear surface section type is NXOpen.Features.VehicleDesign.WheelCoveringBuilderSurfaceSectionType.Adr42 . |
RearHeight | Returns the height of the rear surface section when the rear surface section type is NXOpen.Features.VehicleDesign.WheelCoveringBuilderSurfaceSectionType.Adr42 . |
RearHubcapSelection | Returns the rear hub cap selection. |
RearObjectSelection | Returns the rear object selection. |
RearRadius | Returns the radius of the rear surface section when the rear surface section type is NXOpen.Features.VehicleDesign.WheelCoveringBuilderSurfaceSectionType.CircleSection . |
RearRearAngle | Returns the rear angle of the rear surface section. |
RearRearOffset | Returns the rear offset of the rear surface section when the rear surface section type is NXOpen.Features.VehicleDesign.WheelCoveringBuilderSurfaceSectionType.Adr42 . |
RearSurfacePlane | Returns or sets the surface plane type of the rear surface section. |
RearSurfaceSection | Returns or sets the surface section type of the rear surface section. |
RequirementsControl | Returns or sets the requirements control for standard driven or user defined. |
Standard | Returns or sets the standard used to define the wheel covering. |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
WheelCoveringBuilderPositionType Enumeration | Represents the wheel covering positions. |
WheelCoveringBuilderRequirementsControlType Enumeration | Represents the requirements control types to define the wheel covering. |
WheelCoveringBuilderSurfacePlaneType Enumeration | Represents the type of the surface plane. |
WheelCoveringBuilderSurfaceSectionType Enumeration | Represents the type of the surface section. |
Property Detail¶
DisplayIntersectionCurves¶
-
WheelCoveringBuilder.
DisplayIntersectionCurves
¶ Returns or sets the display of the intersection curves.
-------------------------------------
Getter Method
Signature
DisplayIntersectionCurves
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DisplayIntersectionCurves
Parameters: displayIntersectionCurves (bool) – New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
FrontBottomOffset¶
-
WheelCoveringBuilder.
FrontBottomOffset
¶ Returns the bottom offset of the front surface section when the front surface section type is
NXOpen.Features.VehicleDesign.WheelCoveringBuilderSurfaceSectionType.Adr42
.-------------------------------------
Getter Method
Signature
FrontBottomOffset
Returns: Return type: NXOpen.Expression
New in version NX8.5.0.
License requirements: None.
FrontClearance¶
-
WheelCoveringBuilder.
FrontClearance
¶ Returns the clearance of the front surface section.
-------------------------------------
Getter Method
Signature
FrontClearance
Returns: Return type: NXOpen.Expression
New in version NX8.5.0.
License requirements: None.
FrontFrontAngle¶
-
WheelCoveringBuilder.
FrontFrontAngle
¶ Returns the front angle of the front surface section.
-------------------------------------
Getter Method
Signature
FrontFrontAngle
Returns: Return type: NXOpen.Expression
New in version NX8.5.0.
License requirements: None.
FrontFrontOffset¶
-
WheelCoveringBuilder.
FrontFrontOffset
¶ Returns the front offset of the front surface section when the front surface section type is
NXOpen.Features.VehicleDesign.WheelCoveringBuilderSurfaceSectionType.Adr42
.-------------------------------------
Getter Method
Signature
FrontFrontOffset
Returns: Return type: NXOpen.Expression
New in version NX8.5.0.
License requirements: None.
FrontHeight¶
-
WheelCoveringBuilder.
FrontHeight
¶ Returns the height of the front surface section when front the surface section type is
NXOpen.Features.VehicleDesign.WheelCoveringBuilderSurfaceSectionType.Adr42
.-------------------------------------
Getter Method
Signature
FrontHeight
Returns: Return type: NXOpen.Expression
New in version NX8.5.0.
License requirements: None.
FrontHubcapSelection¶
-
WheelCoveringBuilder.
FrontHubcapSelection
¶ Returns the front hub cap selection.
The collector contains the hub cap faces used to create the front surface section shape.
-------------------------------------
Getter Method
Signature
FrontHubcapSelection
Returns: Return type: NXOpen.ScCollector
New in version NX8.5.0.
License requirements: None.
FrontObjectSelection¶
-
WheelCoveringBuilder.
FrontObjectSelection
¶ Returns the front object selection.
The collector contains the faces used to create the front intersection curves with the front surface section shape.
-------------------------------------
Getter Method
Signature
FrontObjectSelection
Returns: Return type: NXOpen.ScCollector
New in version NX8.5.0.
License requirements: None.
FrontRadius¶
-
WheelCoveringBuilder.
FrontRadius
¶ Returns the radius of the front surface section when the front surface section type is
NXOpen.Features.VehicleDesign.WheelCoveringBuilderSurfaceSectionType.CircleSection
.-------------------------------------
Getter Method
Signature
FrontRadius
Returns: Return type: NXOpen.Expression
New in version NX8.5.0.
License requirements: None.
FrontRearAngle¶
-
WheelCoveringBuilder.
FrontRearAngle
¶ Returns the rear angle of the front surface section.
-------------------------------------
Getter Method
Signature
FrontRearAngle
Returns: Return type: NXOpen.Expression
New in version NX8.5.0.
License requirements: None.
FrontRearOffset¶
-
WheelCoveringBuilder.
FrontRearOffset
¶ Returns the rear offset of the front surface section when the front surface section type is
NXOpen.Features.VehicleDesign.WheelCoveringBuilderSurfaceSectionType.Adr42
.-------------------------------------
Getter Method
Signature
FrontRearOffset
Returns: Return type: NXOpen.Expression
New in version NX8.5.0.
License requirements: None.
FrontSurfacePlane¶
-
WheelCoveringBuilder.
FrontSurfacePlane
¶ Returns or sets the surface plane type of the front surface section.
-------------------------------------
Getter Method
Signature
FrontSurfacePlane
Returns: Return type: NXOpen.Features.VehicleDesign.WheelCoveringBuilderSurfacePlaneType
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FrontSurfacePlane
Parameters: frontSurfacePlane ( NXOpen.Features.VehicleDesign.WheelCoveringBuilderSurfacePlaneType
) –New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
FrontSurfaceSection¶
-
WheelCoveringBuilder.
FrontSurfaceSection
¶ Returns or sets the surface section type of the front surface section.
-------------------------------------
Getter Method
Signature
FrontSurfaceSection
Returns: Return type: NXOpen.Features.VehicleDesign.WheelCoveringBuilderSurfaceSectionType
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FrontSurfaceSection
Parameters: frontSurfaceSection ( NXOpen.Features.VehicleDesign.WheelCoveringBuilderSurfaceSectionType
) –New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
Loading¶
-
WheelCoveringBuilder.
Loading
¶ Returns or sets the loading used in the wheel covering.
-------------------------------------
Getter Method
Signature
Loading
Returns: Return type: str New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Loading
Parameters: loading (str) – New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
Position¶
-
WheelCoveringBuilder.
Position
¶ Returns or sets the wheel covering position.
-------------------------------------
Getter Method
Signature
Position
Returns: Return type: NXOpen.Features.VehicleDesign.WheelCoveringBuilderPositionType
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Position
Parameters: position ( NXOpen.Features.VehicleDesign.WheelCoveringBuilderPositionType
) –New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
RearBottomOffset¶
-
WheelCoveringBuilder.
RearBottomOffset
¶ Returns the bottom offset of the rear surface section when the rear surface section type is
NXOpen.Features.VehicleDesign.WheelCoveringBuilderSurfaceSectionType.Adr42
.-------------------------------------
Getter Method
Signature
RearBottomOffset
Returns: Return type: NXOpen.Expression
New in version NX8.5.0.
License requirements: None.
RearClearance¶
-
WheelCoveringBuilder.
RearClearance
¶ Returns the clearance of the rear surface section.
-------------------------------------
Getter Method
Signature
RearClearance
Returns: Return type: NXOpen.Expression
New in version NX8.5.0.
License requirements: None.
RearDisToWheelCenter¶
-
WheelCoveringBuilder.
RearDisToWheelCenter
¶ Returns the distance to the wheel center when rear surface section type is
NXOpen.Features.VehicleDesign.WheelCoveringBuilderSurfaceSectionType.CircleSection
.-------------------------------------
Getter Method
Signature
RearDisToWheelCenter
Returns: Return type: NXOpen.Expression
New in version NX8.5.0.
License requirements: None.
RearFrontAngle¶
-
WheelCoveringBuilder.
RearFrontAngle
¶ Returns the front angle of the rear surface section.
-------------------------------------
Getter Method
Signature
RearFrontAngle
Returns: Return type: NXOpen.Expression
New in version NX8.5.0.
License requirements: None.
RearFrontOffset¶
-
WheelCoveringBuilder.
RearFrontOffset
¶ Returns the front offset of the rear surface section when the rear surface section type is
NXOpen.Features.VehicleDesign.WheelCoveringBuilderSurfaceSectionType.Adr42
.-------------------------------------
Getter Method
Signature
RearFrontOffset
Returns: Return type: NXOpen.Expression
New in version NX8.5.0.
License requirements: None.
RearHeight¶
-
WheelCoveringBuilder.
RearHeight
¶ Returns the height of the rear surface section when the rear surface section type is
NXOpen.Features.VehicleDesign.WheelCoveringBuilderSurfaceSectionType.Adr42
.-------------------------------------
Getter Method
Signature
RearHeight
Returns: Return type: NXOpen.Expression
New in version NX8.5.0.
License requirements: None.
RearHubcapSelection¶
-
WheelCoveringBuilder.
RearHubcapSelection
¶ Returns the rear hub cap selection.
The collector contains the hub cap faces used to create the rear surface section shape.
-------------------------------------
Getter Method
Signature
RearHubcapSelection
Returns: Return type: NXOpen.ScCollector
New in version NX8.5.0.
License requirements: None.
RearObjectSelection¶
-
WheelCoveringBuilder.
RearObjectSelection
¶ Returns the rear object selection.
The collector contains the faces used to create the rear intersection curves with the rear surface section shape.
-------------------------------------
Getter Method
Signature
RearObjectSelection
Returns: Return type: NXOpen.ScCollector
New in version NX8.5.0.
License requirements: None.
RearRadius¶
-
WheelCoveringBuilder.
RearRadius
¶ Returns the radius of the rear surface section when the rear surface section type is
NXOpen.Features.VehicleDesign.WheelCoveringBuilderSurfaceSectionType.CircleSection
.-------------------------------------
Getter Method
Signature
RearRadius
Returns: Return type: NXOpen.Expression
New in version NX8.5.0.
License requirements: None.
RearRearAngle¶
-
WheelCoveringBuilder.
RearRearAngle
¶ Returns the rear angle of the rear surface section.
-------------------------------------
Getter Method
Signature
RearRearAngle
Returns: Return type: NXOpen.Expression
New in version NX8.5.0.
License requirements: None.
RearRearOffset¶
-
WheelCoveringBuilder.
RearRearOffset
¶ Returns the rear offset of the rear surface section when the rear surface section type is
NXOpen.Features.VehicleDesign.WheelCoveringBuilderSurfaceSectionType.Adr42
.-------------------------------------
Getter Method
Signature
RearRearOffset
Returns: Return type: NXOpen.Expression
New in version NX8.5.0.
License requirements: None.
RearSurfacePlane¶
-
WheelCoveringBuilder.
RearSurfacePlane
¶ Returns or sets the surface plane type of the rear surface section.
-------------------------------------
Getter Method
Signature
RearSurfacePlane
Returns: Return type: NXOpen.Features.VehicleDesign.WheelCoveringBuilderSurfacePlaneType
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RearSurfacePlane
Parameters: rearSurfacePlane ( NXOpen.Features.VehicleDesign.WheelCoveringBuilderSurfacePlaneType
) –New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
RearSurfaceSection¶
-
WheelCoveringBuilder.
RearSurfaceSection
¶ Returns or sets the surface section type of the rear surface section.
-------------------------------------
Getter Method
Signature
RearSurfaceSection
Returns: Return type: NXOpen.Features.VehicleDesign.WheelCoveringBuilderSurfaceSectionType
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RearSurfaceSection
Parameters: rearSurfaceSection ( NXOpen.Features.VehicleDesign.WheelCoveringBuilderSurfaceSectionType
) –New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
RequirementsControl¶
-
WheelCoveringBuilder.
RequirementsControl
¶ Returns or sets the requirements control for standard driven or user defined.
-------------------------------------
Getter Method
Signature
RequirementsControl
Returns: Return type: NXOpen.Features.VehicleDesign.WheelCoveringBuilderRequirementsControlType
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RequirementsControl
Parameters: requirement ( NXOpen.Features.VehicleDesign.WheelCoveringBuilderRequirementsControlType
) –New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
Standard¶
-
WheelCoveringBuilder.
Standard
¶ Returns or sets the standard used to define the wheel covering.
-------------------------------------
Getter Method
Signature
Standard
Returns: Return type: str New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Standard
Parameters: standard (str) – New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
Method Detail¶
Validate¶
-
WheelCoveringBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.