WheelCoveringBuilderPositionType Enumeration¶
NXOpen.Features.VehicleDesign.WheelCoveringBuilder.PositionType is an alias for NXOpen.Features.VehicleDesign.WheelCoveringBuilderPositionType
-
class
NXOpen.Features.VehicleDesign.
WheelCoveringBuilderPositionType
¶ Bases:
object
Represents the wheel covering positions.
Enum Members
Enum Member Enum Member Description Front Creates checking surface for front wheel only Rear Creates checking surface for rear wheel only Both Creates checking surface for both front and rear wheels -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-