WheelCoveringBuilderSurfacePlaneType Enumeration¶
NXOpen.Features.VehicleDesign.WheelCoveringBuilder.SurfacePlaneType is an alias for NXOpen.Features.VehicleDesign.WheelCoveringBuilderSurfacePlaneType
-
class
NXOpen.Features.VehicleDesign.
WheelCoveringBuilderSurfacePlaneType
¶ Bases:
object
Represents the type of the surface plane.
Enum Members
Enum Member Enum Member Description WheelPlane The checking surface is coplanar to the ourside of the wheels PerpendiculartoLoading The checking surface is perpendicular to the active loading plane -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-