CrashBarrierBuilder Class¶
-
class
NXOpen.Features.VehicleDesign.
CrashBarrierBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Features.VehicleDesign.CrashBarrier
builder to create and edit a vehicle design crash barrier.To create a new instance of this class, use
NXOpen.Features.VehicleDesignCollection.CreateCrashBarrierBuilder()
New in version NX8.5.0.
Properties¶
Property | Description |
---|---|
ActiveFront | Returns or sets the value indicating if the front barrier is displayed. |
ActiveRear | Returns or sets the value indicating if the rear barrier is displayed. |
ActiveSide | Returns or sets the value indicating if the side barrier is displayed. |
FrontCrossPosition | Returns or sets the cross position type of front barrier. |
FrontHeightAboveRoad | Returns the expression containing the height above road value of front barrier. |
FrontLoading | Returns or sets the loading applied to the vehicle front used in the crash barrier. |
FrontOverlapPercentage | Returns the expression containing the overlap percentage of front barrier. |
FrontOverlapSide | Returns or sets the overlap side type of front barrier. |
FrontPositionObject | Returns or sets the positioing object type of front barrier. |
FrontSelectPositioningFacetBodies | Returns the positioing facet objects of front barrier. |
FrontSelectPositioningObject | Returns the positioing objects of front barrier. |
FrontShape | Returns or sets the shape type of front barrier. |
FrontShift | Returns the expression containing the shift value of front barrier. |
FrontUserDefineWidth | Returns or sets the user defined width type of front barrier. |
FrontUserDefineWidthValue | Returns the expression containing the user defined width value of front barrier. |
LeftSideSelectPositioningFacetBodies | Returns the left side position facet objects of side barrier. |
LeftSideSelectPositioningObject | Returns the left side position objects of side barrier. |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
RearCrossPosition | Returns or sets the cross position type of rear barrier. |
RearHeightAboveRoad | Returns the expression containing the height above road value of rear barrier. |
RearLoading | Returns or sets the loading applied to the vehicle rear used in the crash barrier. |
RearOverlapPercentage | Returns the expression containing the user defined width value of rear barrier. |
RearOverlapSide | Returns or sets the overlap side type of rear barrier. |
RearPositionObject | Returns or sets the user defined position object type of rear barrier. |
RearSelectPositioningFacetBodies | Returns the user defined position facet objects of rear barrier. |
RearSelectPositioningObject | Returns the user defined position objects of rear barrier. |
RearShape | Returns or sets the shape type of rear barrier. |
RearShift | Returns the expression containing the shift value of rear barrier. |
RearUserDefineWidth | Returns or sets the user defined width type of rear barrier. |
RearUserDefineWidthValue | Returns the expression containing the user defined width value of rear barrier. |
RequirementsControl | Returns or sets the requirements control for standard driven or user defined. |
RightSideSelectPositioningFacetBodies | Returns the right side position facet objects of side barrier. |
RightSideSelectPositioningObject | Returns the right side position objects of side barrier. |
SideCrossPosition | Returns or sets the cross position type of side barrier. |
SideHeightAboveRoad | Returns the expression containing the height above road value of side barrier. |
SideLoading | Returns or sets the loading applied to the vehicle side used in the crash barrier. |
SideOverlapPercentage | Returns the expression containing the overlap percentage of side barrier. |
SideOverlapSide | Returns or sets the overlap side type of side barrier. |
SidePosition | Returns or sets the position type of side barrier. |
SidePositionObject | Returns or sets the side position object type of side barrier. |
SideShape | Returns or sets the shape type of side barrier. |
SideShift | Returns the expression containing the shift value of side barrier. |
SideUserDefineLength | Returns or sets the user defined width type of side barrier. |
SideUserDefineLengthValue | Returns the expression containing the user defined width value of side barrier. |
Standard | Returns or sets the standard used to define the crash barrier. |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
CrashBarrierBuilderCrossPositionType Enumeration | Represents the cross position types. |
CrashBarrierBuilderOverlapSideType Enumeration | Represents the overlap side types for the front and rear barriers. |
CrashBarrierBuilderPositionObjectType Enumeration | Represents the position object types. |
CrashBarrierBuilderRequirementsControlsControlType Enumeration | Represents the requirements control types to define the crash barrier. |
CrashBarrierBuilderShapeType Enumeration | Represents the shape types. |
CrashBarrierBuilderSideOverlapSideType Enumeration | Represents the overlap side types for side barrier. |
CrashBarrierBuilderSidePositionType Enumeration | Represents the position types for side barrier. |
Property Detail¶
ActiveFront¶
-
CrashBarrierBuilder.
ActiveFront
¶ Returns or sets the value indicating if the front barrier is displayed.
-------------------------------------
Getter Method
Signature
ActiveFront
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ActiveFront
Parameters: activeFront (bool) – New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
ActiveRear¶
-
CrashBarrierBuilder.
ActiveRear
¶ Returns or sets the value indicating if the rear barrier is displayed.
-------------------------------------
Getter Method
Signature
ActiveRear
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ActiveRear
Parameters: activeRear (bool) – New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
ActiveSide¶
-
CrashBarrierBuilder.
ActiveSide
¶ Returns or sets the value indicating if the side barrier is displayed.
-------------------------------------
Getter Method
Signature
ActiveSide
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ActiveSide
Parameters: activeSide (bool) – New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
FrontCrossPosition¶
-
CrashBarrierBuilder.
FrontCrossPosition
¶ Returns or sets the cross position type of front barrier.
-------------------------------------
Getter Method
Signature
FrontCrossPosition
Returns: Return type: NXOpen.Features.VehicleDesign.CrashBarrierBuilderCrossPositionType
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FrontCrossPosition
Parameters: frontCrossPosition ( NXOpen.Features.VehicleDesign.CrashBarrierBuilderCrossPositionType
) –New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
FrontHeightAboveRoad¶
-
CrashBarrierBuilder.
FrontHeightAboveRoad
¶ Returns the expression containing the height above road value of front barrier.
-------------------------------------
Getter Method
Signature
FrontHeightAboveRoad
Returns: Return type: NXOpen.Expression
New in version NX8.5.0.
License requirements: None.
FrontLoading¶
-
CrashBarrierBuilder.
FrontLoading
¶ Returns or sets the loading applied to the vehicle front used in the crash barrier.
-------------------------------------
Getter Method
Signature
FrontLoading
Returns: Return type: str New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FrontLoading
Parameters: frontLoading (str) – New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
FrontOverlapPercentage¶
-
CrashBarrierBuilder.
FrontOverlapPercentage
¶ Returns the expression containing the overlap percentage of front barrier.
-------------------------------------
Getter Method
Signature
FrontOverlapPercentage
Returns: Return type: NXOpen.Expression
New in version NX8.5.0.
License requirements: None.
FrontOverlapSide¶
-
CrashBarrierBuilder.
FrontOverlapSide
¶ Returns or sets the overlap side type of front barrier.
-------------------------------------
Getter Method
Signature
FrontOverlapSide
Returns: Return type: NXOpen.Features.VehicleDesign.CrashBarrierBuilderOverlapSideType
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FrontOverlapSide
Parameters: frontOverlapSide ( NXOpen.Features.VehicleDesign.CrashBarrierBuilderOverlapSideType
) –New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
FrontPositionObject¶
-
CrashBarrierBuilder.
FrontPositionObject
¶ Returns or sets the positioing object type of front barrier.
-------------------------------------
Getter Method
Signature
FrontPositionObject
Returns: Return type: NXOpen.Features.VehicleDesign.CrashBarrierBuilderPositionObjectType
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FrontPositionObject
Parameters: frontPositionObject ( NXOpen.Features.VehicleDesign.CrashBarrierBuilderPositionObjectType
) –New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
FrontSelectPositioningFacetBodies¶
-
CrashBarrierBuilder.
FrontSelectPositioningFacetBodies
¶ Returns the positioing facet objects of front barrier.
-------------------------------------
Getter Method
Signature
FrontSelectPositioningFacetBodies
Returns: Return type: NXOpen.SelectNXObjectList
New in version NX11.0.0.
License requirements: None.
FrontSelectPositioningObject¶
-
CrashBarrierBuilder.
FrontSelectPositioningObject
¶ Returns the positioing objects of front barrier.
-------------------------------------
Getter Method
Signature
FrontSelectPositioningObject
Returns: Return type: NXOpen.ScCollector
New in version NX8.5.0.
License requirements: None.
FrontShape¶
-
CrashBarrierBuilder.
FrontShape
¶ Returns or sets the shape type of front barrier.
-------------------------------------
Getter Method
Signature
FrontShape
Returns: Return type: NXOpen.Features.VehicleDesign.CrashBarrierBuilderShapeType
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FrontShape
Parameters: frontShap ( NXOpen.Features.VehicleDesign.CrashBarrierBuilderShapeType
) –New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
FrontShift¶
-
CrashBarrierBuilder.
FrontShift
¶ Returns the expression containing the shift value of front barrier.
-------------------------------------
Getter Method
Signature
FrontShift
Returns: Return type: NXOpen.Expression
New in version NX8.5.0.
License requirements: None.
FrontUserDefineWidth¶
-
CrashBarrierBuilder.
FrontUserDefineWidth
¶ Returns or sets the user defined width type of front barrier.
-------------------------------------
Getter Method
Signature
FrontUserDefineWidth
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FrontUserDefineWidth
Parameters: frontUserDefineWidth (bool) – New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
FrontUserDefineWidthValue¶
-
CrashBarrierBuilder.
FrontUserDefineWidthValue
¶ Returns the expression containing the user defined width value of front barrier.
-------------------------------------
Getter Method
Signature
FrontUserDefineWidthValue
Returns: Return type: NXOpen.Expression
New in version NX8.5.0.
License requirements: None.
LeftSideSelectPositioningFacetBodies¶
-
CrashBarrierBuilder.
LeftSideSelectPositioningFacetBodies
¶ Returns the left side position facet objects of side barrier.
-------------------------------------
Getter Method
Signature
LeftSideSelectPositioningFacetBodies
Returns: Return type: NXOpen.SelectNXObjectList
New in version NX11.0.0.
License requirements: None.
LeftSideSelectPositioningObject¶
-
CrashBarrierBuilder.
LeftSideSelectPositioningObject
¶ Returns the left side position objects of side barrier.
-------------------------------------
Getter Method
Signature
LeftSideSelectPositioningObject
Returns: Return type: NXOpen.ScCollector
New in version NX8.5.0.
License requirements: None.
RearCrossPosition¶
-
CrashBarrierBuilder.
RearCrossPosition
¶ Returns or sets the cross position type of rear barrier.
-------------------------------------
Getter Method
Signature
RearCrossPosition
Returns: Return type: NXOpen.Features.VehicleDesign.CrashBarrierBuilderCrossPositionType
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RearCrossPosition
Parameters: rearCrossPosition ( NXOpen.Features.VehicleDesign.CrashBarrierBuilderCrossPositionType
) –New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
RearHeightAboveRoad¶
-
CrashBarrierBuilder.
RearHeightAboveRoad
¶ Returns the expression containing the height above road value of rear barrier.
-------------------------------------
Getter Method
Signature
RearHeightAboveRoad
Returns: Return type: NXOpen.Expression
New in version NX8.5.0.
License requirements: None.
RearLoading¶
-
CrashBarrierBuilder.
RearLoading
¶ Returns or sets the loading applied to the vehicle rear used in the crash barrier.
-------------------------------------
Getter Method
Signature
RearLoading
Returns: Return type: str New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RearLoading
Parameters: rearLoading (str) – New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
RearOverlapPercentage¶
-
CrashBarrierBuilder.
RearOverlapPercentage
¶ Returns the expression containing the user defined width value of rear barrier.
-------------------------------------
Getter Method
Signature
RearOverlapPercentage
Returns: Return type: NXOpen.Expression
New in version NX8.5.0.
License requirements: None.
RearOverlapSide¶
-
CrashBarrierBuilder.
RearOverlapSide
¶ Returns or sets the overlap side type of rear barrier.
-------------------------------------
Getter Method
Signature
RearOverlapSide
Returns: Return type: NXOpen.Features.VehicleDesign.CrashBarrierBuilderOverlapSideType
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RearOverlapSide
Parameters: rearOverlapSide ( NXOpen.Features.VehicleDesign.CrashBarrierBuilderOverlapSideType
) –New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
RearPositionObject¶
-
CrashBarrierBuilder.
RearPositionObject
¶ Returns or sets the user defined position object type of rear barrier.
-------------------------------------
Getter Method
Signature
RearPositionObject
Returns: Return type: NXOpen.Features.VehicleDesign.CrashBarrierBuilderPositionObjectType
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RearPositionObject
Parameters: rearPositionObject ( NXOpen.Features.VehicleDesign.CrashBarrierBuilderPositionObjectType
) –New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
RearSelectPositioningFacetBodies¶
-
CrashBarrierBuilder.
RearSelectPositioningFacetBodies
¶ Returns the user defined position facet objects of rear barrier.
-------------------------------------
Getter Method
Signature
RearSelectPositioningFacetBodies
Returns: Return type: NXOpen.SelectNXObjectList
New in version NX11.0.0.
License requirements: None.
RearSelectPositioningObject¶
-
CrashBarrierBuilder.
RearSelectPositioningObject
¶ Returns the user defined position objects of rear barrier.
-------------------------------------
Getter Method
Signature
RearSelectPositioningObject
Returns: Return type: NXOpen.ScCollector
New in version NX8.5.0.
License requirements: None.
RearShape¶
-
CrashBarrierBuilder.
RearShape
¶ Returns or sets the shape type of rear barrier.
-------------------------------------
Getter Method
Signature
RearShape
Returns: Return type: NXOpen.Features.VehicleDesign.CrashBarrierBuilderShapeType
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RearShape
Parameters: rearShape ( NXOpen.Features.VehicleDesign.CrashBarrierBuilderShapeType
) –New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
RearShift¶
-
CrashBarrierBuilder.
RearShift
¶ Returns the expression containing the shift value of rear barrier.
-------------------------------------
Getter Method
Signature
RearShift
Returns: Return type: NXOpen.Expression
New in version NX8.5.0.
License requirements: None.
RearUserDefineWidth¶
-
CrashBarrierBuilder.
RearUserDefineWidth
¶ Returns or sets the user defined width type of rear barrier.
-------------------------------------
Getter Method
Signature
RearUserDefineWidth
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RearUserDefineWidth
Parameters: rearUserDefineWidth (bool) – New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
RearUserDefineWidthValue¶
-
CrashBarrierBuilder.
RearUserDefineWidthValue
¶ Returns the expression containing the user defined width value of rear barrier.
-------------------------------------
Getter Method
Signature
RearUserDefineWidthValue
Returns: Return type: NXOpen.Expression
New in version NX8.5.0.
License requirements: None.
RequirementsControl¶
-
CrashBarrierBuilder.
RequirementsControl
¶ Returns or sets the requirements control for standard driven or user defined.
-------------------------------------
Getter Method
Signature
RequirementsControl
Returns: Return type: NXOpen.Features.VehicleDesign.CrashBarrierBuilderRequirementsControlsControlType
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RequirementsControl
Parameters: requirement ( NXOpen.Features.VehicleDesign.CrashBarrierBuilderRequirementsControlsControlType
) –New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
RightSideSelectPositioningFacetBodies¶
-
CrashBarrierBuilder.
RightSideSelectPositioningFacetBodies
¶ Returns the right side position facet objects of side barrier.
-------------------------------------
Getter Method
Signature
RightSideSelectPositioningFacetBodies
Returns: Return type: NXOpen.SelectNXObjectList
New in version NX11.0.0.
License requirements: None.
RightSideSelectPositioningObject¶
-
CrashBarrierBuilder.
RightSideSelectPositioningObject
¶ Returns the right side position objects of side barrier.
-------------------------------------
Getter Method
Signature
RightSideSelectPositioningObject
Returns: Return type: NXOpen.ScCollector
New in version NX8.5.0.
License requirements: None.
SideCrossPosition¶
-
CrashBarrierBuilder.
SideCrossPosition
¶ Returns or sets the cross position type of side barrier.
-------------------------------------
Getter Method
Signature
SideCrossPosition
Returns: Return type: NXOpen.Features.VehicleDesign.CrashBarrierBuilderCrossPositionType
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SideCrossPosition
Parameters: sideCrossPosition ( NXOpen.Features.VehicleDesign.CrashBarrierBuilderCrossPositionType
) –New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
SideHeightAboveRoad¶
-
CrashBarrierBuilder.
SideHeightAboveRoad
¶ Returns the expression containing the height above road value of side barrier.
-------------------------------------
Getter Method
Signature
SideHeightAboveRoad
Returns: Return type: NXOpen.Expression
New in version NX8.5.0.
License requirements: None.
SideLoading¶
-
CrashBarrierBuilder.
SideLoading
¶ Returns or sets the loading applied to the vehicle side used in the crash barrier.
-------------------------------------
Getter Method
Signature
SideLoading
Returns: Return type: str New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SideLoading
Parameters: sideLoading (str) – New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
SideOverlapPercentage¶
-
CrashBarrierBuilder.
SideOverlapPercentage
¶ Returns the expression containing the overlap percentage of side barrier.
-------------------------------------
Getter Method
Signature
SideOverlapPercentage
Returns: Return type: NXOpen.Expression
New in version NX8.5.0.
License requirements: None.
SideOverlapSide¶
-
CrashBarrierBuilder.
SideOverlapSide
¶ Returns or sets the overlap side type of side barrier.
-------------------------------------
Getter Method
Signature
SideOverlapSide
Returns: Return type: NXOpen.Features.VehicleDesign.CrashBarrierBuilderSideOverlapSideType
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SideOverlapSide
Parameters: sideOverlapSide ( NXOpen.Features.VehicleDesign.CrashBarrierBuilderSideOverlapSideType
) –New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
SidePosition¶
-
CrashBarrierBuilder.
SidePosition
¶ Returns or sets the position type of side barrier.
-------------------------------------
Getter Method
Signature
SidePosition
Returns: Return type: NXOpen.Features.VehicleDesign.CrashBarrierBuilderSidePositionType
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SidePosition
Parameters: sidePosition ( NXOpen.Features.VehicleDesign.CrashBarrierBuilderSidePositionType
) –New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
SidePositionObject¶
-
CrashBarrierBuilder.
SidePositionObject
¶ Returns or sets the side position object type of side barrier.
-------------------------------------
Getter Method
Signature
SidePositionObject
Returns: Return type: NXOpen.Features.VehicleDesign.CrashBarrierBuilderPositionObjectType
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SidePositionObject
Parameters: sidePositionObject ( NXOpen.Features.VehicleDesign.CrashBarrierBuilderPositionObjectType
) –New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
SideShape¶
-
CrashBarrierBuilder.
SideShape
¶ Returns or sets the shape type of side barrier.
-------------------------------------
Getter Method
Signature
SideShape
Returns: Return type: NXOpen.Features.VehicleDesign.CrashBarrierBuilderShapeType
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SideShape
Parameters: sideShape ( NXOpen.Features.VehicleDesign.CrashBarrierBuilderShapeType
) –New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
SideShift¶
-
CrashBarrierBuilder.
SideShift
¶ Returns the expression containing the shift value of side barrier.
-------------------------------------
Getter Method
Signature
SideShift
Returns: Return type: NXOpen.Expression
New in version NX8.5.0.
License requirements: None.
SideUserDefineLength¶
-
CrashBarrierBuilder.
SideUserDefineLength
¶ Returns or sets the user defined width type of side barrier.
-------------------------------------
Getter Method
Signature
SideUserDefineLength
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SideUserDefineLength
Parameters: sideUserDefineLength (bool) – New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
SideUserDefineLengthValue¶
-
CrashBarrierBuilder.
SideUserDefineLengthValue
¶ Returns the expression containing the user defined width value of side barrier.
-------------------------------------
Getter Method
Signature
SideUserDefineLengthValue
Returns: Return type: NXOpen.Expression
New in version NX8.5.0.
License requirements: None.
Standard¶
-
CrashBarrierBuilder.
Standard
¶ Returns or sets the standard used to define the crash barrier.
-------------------------------------
Getter Method
Signature
Standard
Returns: Return type: str New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Standard
Parameters: standard (str) – New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
Method Detail¶
Validate¶
-
CrashBarrierBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.