CrashBarrierBuilderRequirementsControlsControlType Enumeration

NXOpen.Features.VehicleDesign.CrashBarrierBuilder.RequirementsControlsControlType is an alias for NXOpen.Features.VehicleDesign.CrashBarrierBuilderRequirementsControlsControlType

class NXOpen.Features.VehicleDesign.CrashBarrierBuilderRequirementsControlsControlType

Bases: object

Represents the requirements control types to define the crash barrier.

Enum Members

Enum Member Enum Member Description
StandardDriven
UserDefined
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.