CrashBarrierBuilderPositionObjectType Enumeration

NXOpen.Features.VehicleDesign.CrashBarrierBuilder.PositionObjectType is an alias for NXOpen.Features.VehicleDesign.CrashBarrierBuilderPositionObjectType

class NXOpen.Features.VehicleDesign.CrashBarrierBuilderPositionObjectType

Bases: object

Represents the position object types.

Enum Members

Enum Member Enum Member Description
BaseData
VehicleObject
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.